2023-04-24 1:15 AM
Hi,
I'm having some trouble with trying to correct the RTC drift on a STM32F439NIHx. I've enabled the REF_IN and provided a 50Hz signal on the pin, but the RTC still drifts by around 1s per day.
I've also tested that the 50Hz signal is correctly received by changing the pin to an external interrupt and correctly generated 50 interrupts per seconds.
Am I missing something or doing something wrong in the setup:
Enabling the RTC and the ref in :
RTC_HandleTypeDef hrtc = RTC_HandleTypeDef();
hrtc.Instance = RTC;
hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
hrtc.Init.AsynchPrediv = RTC_ASYNCH_PREDIV;
hrtc.Init.SynchPrediv = RTC_SYNCH_PREDIV;
hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
if (HAL_RTC_Init(hrtc) != HAL_OK)
{
Error_Handler();
}
if (HAL_RTCEx_EnableBypassShadow(hrtc) != HAL_OK)
{
Error_Handler();
}
if (HAL_RTCEx_SetRefClock(hrtc) != HAL_OK)
{
Error_Handler();
}and the HAL_RTC_MspInit function:
void HAL_RTC_MspInit(RTC_HandleTypeDef* hrtc) {
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
GPIO_InitTypeDef GPIO_InitStruct = {0};
/**RTC GPIO Configuration
PB15 ------> RTC_REFIN
*/
GPIO_InitStruct.Pin = GPIO_PIN_15;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
HAL_GPIO_LockPin(GPIOB, RTC_REF_IN_PIN); // Lock Pin configuration
// Configure LSE as RTC clock source
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI | RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.LSIState = RCC_LSI_OFF;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) {
// Initialization Error
return;
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_RTC;
PeriphClkInitStruct.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK) {
// Initialization Error
return;
}
// Enable RTC peripheral Clocks
__HAL_RCC_RTC_ENABLE();
// Configure the NVIC for RTC Alarm
HAL_NVIC_SetPriority(RTC_Alarm_IRQn, 0x0F, 0);
HAL_NVIC_EnableIRQ(RTC_Alarm_IRQn);
}
Solved! Go to Solution.
2023-04-24 7:02 AM
> GPIO_InitStruct.Pin = GPIO_PIN_15;
> GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
According to Datasheet, RTC_REFIN is PB15 AF0, so you want to set it to Alternate Function.
JW
2023-04-24 1:22 AM
I don't have experience with the REF_IN facility, but 1s/day is around 10ppm, are you sure your 50Hz source more precise than that?
What's the raw precision of the LSE?
At any case, read out and check/post content of RTC and RCC_BDTR registers.
JW
2023-04-24 2:01 AM
The 50Hz source is a lot more precise than that, under 0.01ppm.
I'm not sure about the LSE precision, but given we get the 1s/day drift also when we don't set the REF_IN, probably around 10ppm.
I don't see a RCC_BDTR register, but RCC_BDCR has the value 0x00008103
The RTC registers are as follow:
RTC_CR 0x00001130
RTC_ISR 0x00000017
RTC_PRER 0x007F00FF
RTC_WURT 0X0000FFFF
RTC_CALIBR 0X00000000
RTC_ALRMAR 0XC1808080
RTC_ALRMBR 0X00000000
RTC_ALRMASSR 0X0F000000
RTC_RESERVED7 0X00002000
RTC_BKP0R 0X000032F2with the other RTC registers at 0x00000000, or changing for TR, DR and SSR
2023-04-24 3:20 AM
> RTC_BKP0R 0X000032F2
Oh, that unnecessary Cube "signature".
Which makes me to ask: do you power-on/reset the device within the 24-hour period? If yes, couldn't it be this?
JW
2023-04-24 3:54 AM
No, though I also have that issue with the reset, in this case the drift happens without any reset on the device during the test.. (The drift is also forward, gaining 1s/day, so it can't be caused by a similar issue, since it would then lose 1s/day).
2023-04-24 5:22 AM
>under 0.01ppm
thats 10e-8 -- so you have an atomic clock around all the time ?
2023-04-24 5:40 AM
GPS or AC Grid synchronization..
2023-04-24 6:01 AM
obvious ... but : afaik GPS makes 1 Hz output, not 50.
and grid ... now i looked: actual -240ppm away, so "under 0.01ppm" you might get in 10..20 month average, never in 24 h. https://www.netzfrequenzmessung.de/
that's why I'm puzzled...
2023-04-24 6:37 AM
The 50Hz signal I use for the REF_IN is indeed provided by an atomic clock.
2023-04-24 7:02 AM
> GPIO_InitStruct.Pin = GPIO_PIN_15;
> GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
According to Datasheet, RTC_REFIN is PB15 AF0, so you want to set it to Alternate Function.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.