2023-04-27 8:25 AM
Hello,
I'm trying to configure the GPDMA1 to transfer conversion results from ADC1 and ADC4 to two results buffers using two separate GPDMA1 channels on a STM32U575. The DMA channels are both configured as 'Standard Request Mode' with 'Circular Mode' enabled and the request set to their respective ADCs. Both ADCs are set to scan continuously over the enabled analog channels.
This all seems to work as expected provided that the two DMA channels are set to use different ports for transfer. If I set both DMA channels to use port 0 (which appears to be recommended for peripheral to memory transfers) or port 1 then the data copied by the DMA to each results buffer in memory gets muddled up rather than appearing at the expected buffer index. It looks like the destination addresses aren't being incremented correctly as I can see the conversion results moving around in the buffer over time.
From reading the manuals and application notes, I can't understand why two DMA channels both using port 0 should be an issue. Hopefully someone can enlighten me! I'd like to be sure that I won't have further issues if I try to use a third DMA channel for another peripheral.
Here's the ADC init code in main.c:
static void MX_ADC1_Init(void)
{
ADC_ChannelConfTypeDef sConfig = {0};
/** Common config
*/
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV4;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.GainCompensation = 0;
hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc1.Init.LowPowerAutoWait = DISABLE;
hadc1.Init.ContinuousConvMode = ENABLE;
hadc1.Init.NbrOfConversion = 16;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.DMAContinuousRequests = DISABLE;
hadc1.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
hadc1.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
hadc1.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR;
hadc1.Init.OversamplingMode = DISABLE;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_5CYCLE;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_2;
sConfig.Rank = ADC_REGULAR_RANK_2;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_3;
sConfig.Rank = ADC_REGULAR_RANK_3;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
...
}
static void MX_ADC4_Init(void)
{
ADC_ChannelConfTypeDef sConfig = {0};
/** Common config
*/
hadc4.Instance = ADC4;
hadc4.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV4;
hadc4.Init.Resolution = ADC_RESOLUTION_12B;
hadc4.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc4.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD;
hadc4.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc4.Init.LowPowerAutoPowerOff = ADC_LOW_POWER_NONE;
hadc4.Init.LowPowerAutoWait = DISABLE;
hadc4.Init.ContinuousConvMode = ENABLE;
hadc4.Init.NbrOfConversion = 1;
hadc4.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc4.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc4.Init.DMAContinuousRequests = ENABLE;
hadc4.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_LOW;
hadc4.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
hadc4.Init.SamplingTimeCommon1 = ADC4_SAMPLETIME_7CYCLES_5;
hadc4.Init.SamplingTimeCommon2 = ADC4_SAMPLETIME_7CYCLES_5;
hadc4.Init.OversamplingMode = DISABLE;
if (HAL_ADC_Init(&hadc4) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_6;
sConfig.Rank = ADC4_RANK_CHANNEL_NUMBER;
sConfig.SamplingTime = ADC4_SAMPLINGTIME_COMMON_1;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc4, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_7;
if (HAL_ADC_ConfigChannel(&hadc4, &sConfig) != HAL_OK)
{
Error_Handler();
}
...
}Here's the ADC/DMA init code in stm32u5xx_hal_msp.c:
void HAL_ADC_MspInit(ADC_HandleTypeDef* hadc)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
DMA_NodeConfTypeDef NodeConfig;
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
if(hadc->Instance==ADC1)
{
...
/* ADC1 DMA Init */
/* GPDMA1_REQUEST_ADC1 Init */
NodeConfig.NodeType = DMA_GPDMA_LINEAR_NODE;
NodeConfig.Init.Request = GPDMA1_REQUEST_ADC1;
NodeConfig.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
NodeConfig.Init.Direction = DMA_PERIPH_TO_MEMORY;
NodeConfig.Init.SrcInc = DMA_SINC_FIXED;
NodeConfig.Init.DestInc = DMA_DINC_INCREMENTED;
NodeConfig.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_WORD;
NodeConfig.Init.DestDataWidth = DMA_DEST_DATAWIDTH_WORD;
NodeConfig.Init.SrcBurstLength = 1;
NodeConfig.Init.DestBurstLength = 1;
NodeConfig.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT1|DMA_DEST_ALLOCATED_PORT1;
NodeConfig.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
NodeConfig.Init.Mode = DMA_NORMAL;
NodeConfig.TriggerConfig.TriggerPolarity = DMA_TRIG_POLARITY_MASKED;
NodeConfig.DataHandlingConfig.DataExchange = DMA_EXCHANGE_NONE;
NodeConfig.DataHandlingConfig.DataAlignment = DMA_DATA_RIGHTALIGN_ZEROPADDED;
if (HAL_DMAEx_List_BuildNode(&NodeConfig, &Node_GPDMA1_Channel10) != HAL_OK)
{
Error_Handler();
}
if (HAL_DMAEx_List_InsertNode(&List_GPDMA1_Channel10, NULL, &Node_GPDMA1_Channel10) != HAL_OK)
{
Error_Handler();
}
if (HAL_DMAEx_List_SetCircularMode(&List_GPDMA1_Channel10) != HAL_OK)
{
Error_Handler();
}
handle_GPDMA1_Channel10.Instance = GPDMA1_Channel10;
handle_GPDMA1_Channel10.InitLinkedList.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT;
handle_GPDMA1_Channel10.InitLinkedList.LinkStepMode = DMA_LSM_FULL_EXECUTION;
handle_GPDMA1_Channel10.InitLinkedList.LinkAllocatedPort = DMA_LINK_ALLOCATED_PORT1;
handle_GPDMA1_Channel10.InitLinkedList.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
handle_GPDMA1_Channel10.InitLinkedList.LinkedListMode = DMA_LINKEDLIST_CIRCULAR;
if (HAL_DMAEx_List_Init(&handle_GPDMA1_Channel10) != HAL_OK)
{
Error_Handler();
}
if (HAL_DMAEx_List_LinkQ(&handle_GPDMA1_Channel10, &List_GPDMA1_Channel10) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hadc, DMA_Handle, handle_GPDMA1_Channel10);
if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel10, DMA_CHANNEL_NPRIV) != HAL_OK)
{
Error_Handler();
}
}
else if(hadc->Instance==ADC4)
{
...
/* ADC4 DMA Init */
/* GPDMA1_REQUEST_ADC4 Init */
NodeConfig.NodeType = DMA_GPDMA_LINEAR_NODE;
NodeConfig.Init.Request = GPDMA1_REQUEST_ADC4;
NodeConfig.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
NodeConfig.Init.Direction = DMA_PERIPH_TO_MEMORY;
NodeConfig.Init.SrcInc = DMA_SINC_FIXED;
NodeConfig.Init.DestInc = DMA_DINC_INCREMENTED;
NodeConfig.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_HALFWORD;
NodeConfig.Init.DestDataWidth = DMA_DEST_DATAWIDTH_WORD;
NodeConfig.Init.SrcBurstLength = 1;
NodeConfig.Init.DestBurstLength = 1;
NodeConfig.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT0|DMA_DEST_ALLOCATED_PORT0;
NodeConfig.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
NodeConfig.Init.Mode = DMA_NORMAL;
NodeConfig.TriggerConfig.TriggerPolarity = DMA_TRIG_POLARITY_MASKED;
NodeConfig.DataHandlingConfig.DataExchange = DMA_EXCHANGE_NONE;
NodeConfig.DataHandlingConfig.DataAlignment = DMA_DATA_RIGHTALIGN_ZEROPADDED;
if (HAL_DMAEx_List_BuildNode(&NodeConfig, &Node_GPDMA1_Channel11) != HAL_OK)
{
Error_Handler();
}
if (HAL_DMAEx_List_InsertNode(&List_GPDMA1_Channel11, NULL, &Node_GPDMA1_Channel11) != HAL_OK)
{
Error_Handler();
}
if (HAL_DMAEx_List_SetCircularMode(&List_GPDMA1_Channel11) != HAL_OK)
{
Error_Handler();
}
handle_GPDMA1_Channel11.Instance = GPDMA1_Channel11;
handle_GPDMA1_Channel11.InitLinkedList.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT;
handle_GPDMA1_Channel11.InitLinkedList.LinkStepMode = DMA_LSM_FULL_EXECUTION;
handle_GPDMA1_Channel11.InitLinkedList.LinkAllocatedPort = DMA_LINK_ALLOCATED_PORT0;
handle_GPDMA1_Channel11.InitLinkedList.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
handle_GPDMA1_Channel11.InitLinkedList.LinkedListMode = DMA_LINKEDLIST_CIRCULAR;
if (HAL_DMAEx_List_Init(&handle_GPDMA1_Channel11) != HAL_OK)
{
Error_Handler();
}
if (HAL_DMAEx_List_LinkQ(&handle_GPDMA1_Channel11, &List_GPDMA1_Channel11) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hadc, DMA_Handle, handle_GPDMA1_Channel11);
if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel11, DMA_CHANNEL_NPRIV) != HAL_OK)
{
Error_Handler();
}
}
}Here's where the ADCs are started:
/* Start the ADC conversions */
if (HAL_ADC_Start_DMA(&hadc1, (uint32_t*) Adc1ResultRaw, ADC1_CHANNEL_NUMBER) != HAL_OK) {
/* Error */
}
if (HAL_ADC_Start_DMA(&hadc4, (uint32_t *)Adc4ResultRaw, ADC4_CHANNEL_NUMBER) != HAL_OK)
{
/* Error */
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.