STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

The DMA transfer only the first byte from ADC1 (STM32H735)

I configure the ADC1 of the STM32H735 like bellow:The ADC Clock = 20MHzADC_HandleTypeDef hadc1; DMA_HandleTypeDef hdma_adc1;   /* ADC1 init function */ void MX_ADC1_Init(void) {   /* USER CODE BEGIN ADC1_Init 0 */   /* USER CODE END ADC1_Init 0 *...

_legacyfs_online_stmicro_images_0693W00000biUC8QAM.png _legacyfs_online_stmicro_images_0693W00000biUKvQAM.png
Saif by Associate II
  • 7147 Views
  • 19 replies
  • 0 kudos

STM32F DAC not driving voltage to more than 0V

Hello,I am using a STM32F429I-Discovery board for a project involving the use of both DAC channels. I am using the Peripheral driver library for faster coding. Despite having configured everything as specified in the docs and the library I cannot get...

gives by Associate
  • 1712 Views
  • 3 replies
  • 1 kudos

Capture egdedirection on input capture with dma

Hello,i am using the STM32F410CBUx and want to detect rising and falling edges with the Timer 5.I get these values with the help of the DMA because the signal edges are close together and i need accurate meassurments. The edges occure all in a short ...

PDieh.1 by Associate III
  • 4435 Views
  • 8 replies
  • 1 kudos

How to use an external signal to trigger ADC on H755ZI?

 Hello,As the title says, I need to use the ADC's external trigger designator pin to trigger the transition. I have done the necessary steps on Cubemx but my code still cannot work.Looking forward to hearing from the forum.Thanks,HAILV /* USER CODE E...

_legacyfs_online_stmicro_images_0693W00000bhp5LQAQ.png
Ruồi by Associate III
  • 1423 Views
  • 1 replies
  • 1 kudos

Resolved! Error in UM2861

at page 26 :"The X3 crystal has the following characteristics: 32.768 kHz"it should be X2 instead of X3

nicolas by Senior II
  • 1433 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.