STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to debug Timer interrupt

Hi all, Is there any method to debug timer interrupts using VSCode? I am currently using the STM32G4 series. it would be really nice if anyone can point out a way to debug.I am using OpenOCD. Thanks Roshan

Roshan by Associate III
  • 4617 Views
  • 4 replies
  • 0 kudos

cubeIDE, stm32F407ZGT6 with HAL. Config. generated by IOC. SEGGER J-Link debugger. Most basic program w/ 1 GPIO pin driving a LED based on HAL_SysTicks. HSE 12 MHz.HCLK 168 MHz.(or any other freq. same behavior).

Problem: During HALL_Init(), when executing macro __HAL_RCC_SYSCFG_CLK_ENABLE() the interrupt vector table is overwriten w/ garbage.At first interrupt generated by TimeBase (SysTicks) debugger gets a SIGTRAP @ 0x1fff3744 outside of program code. Int...

JIVAN.1 by Associate
  • 2080 Views
  • 3 replies
  • 0 kudos

Resolved! CAN Receive Interruption not working on STM32F0-DISCOVERY

Hello,I am trying to set up a CAN Data Frame receive interruption on a STM32F0-DISCOVERY board. The interruption seems to jump for all other IER register elements, but not for the RX. Stopping the processor execution on debug and checking the status ...

ATeso.1 by Associate
  • 1981 Views
  • 3 replies
  • 1 kudos

Resolved! A way of distinguishing between different series of STM32 ?

Hi!I am working on a project with stm32h757 and soon we will be switching to stm32h747. i need a way to know (using SW) on which processor i am working with.is there some type of register that holds this info?I saw the 96b UID but as i understad it ...

yuri CH by Senior
  • 3978 Views
  • 5 replies
  • 0 kudos

How to add Cortex-M33 to TrueSTUDIO ?

I know TrueSTUDIO is tagged as obsolete, but I like to use it.The STM32H5 use Cortex-M33 core, then how to add M33 support?I already upgraded TrueSTUDIO to support GCC 10.3.1 and recent loaders and SVD files. It would be nice to use M33 cores with Tr...

_legacyfs_online_stmicro_images_0693W00000blDmmQAE.png

Resolved! Bit-banged I2S on STM32F103

Hello everybody,I am trying to bit-bang an I2S interface on an STM32F103 at 72MHz using TIM2.Am I way too optimistic to get a 3MHz "clock" out on a pin? The fastest I can seem to get it is at 90kHz.I have set the "prescaler" of TIM2 to "0" and "1".An...

PGild.1 by Associate III
  • 5570 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.