2023-05-30 7:05 AM
Hello,
I am trying to set up a CAN Data Frame receive interruption on a STM32F0-DISCOVERY board. The interruption seems to jump for all other IER register elements, but not for the RX. Stopping the processor execution on debug and checking the status of the RX registers, it seems not receive any kind of data, even though there is a source of data frames in the BUS.
I have tried also to set up the CAN interface in Loopback mode to test the system alone. The same result is obtained.
Has anybody had the same problem? Any idea why the RX registers are not being filled with the bus date?
Thanks in advance,
Solved! Go to Solution.
2023-05-30 8:47 AM
Hello,
It could be filter config issue. If the filter is not well configured you will never receive the data.
You can inspire from any CAN example provided in STM32CubeF0.
Example from the path STM32072B_EVAL\Examples\CAN\CAN_Networking
2023-05-30 8:47 AM
Hello,
It could be filter config issue. If the filter is not well configured you will never receive the data.
You can inspire from any CAN example provided in STM32CubeF0.
Example from the path STM32072B_EVAL\Examples\CAN\CAN_Networking
2023-05-30 11:10 PM
Hello again,
You were right, the problem came from not configuring the filters. I used the example you mentioned as base and now the CAN is able to receive data.
Thanks a lot.
2023-05-31 9:29 AM
Thank you for the confirmation.
I invite you to close this thread by clicking "Select as best" my answer to help others to find the answer later-on.
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.