STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F4 - Fade and Loop Debugging Help

Greetings,I have been working with the STM32F407ZG and a KnobG Click from MikroElectronica. I read the datasheet for the PCA9956B and have managed to address the device successfully at the address of 0x70. Now then according to the usage I have seen ...

Resolved! STM32 Ethernet RMII set up issues

Hey all, I've been working on this issue for about a week and am still not gaining any traction. I am trying to set up the RMII for the STM32H723ZG eval board (I cannot use the MII as we are using the pins for other peripherals).The LwIP TCP echo wor...

cjbruff_1-1689880164929.png cjbruff_2-1689880180087.png cjbruff_3-1689880193359.png cjbruff_4-1689880211886.png
cjbruff by Associate II
  • 5713 Views
  • 5 replies
  • 0 kudos

Resolved! STM32G03 DMA initialization causing uwanted effects on Systick

Hi everyone,Im havinga annoying problem, im trying to inialize the DMA with the ADC , on my custom board. when a initlize it, it works fine, i get the 3 values of the trhee adc channel stored on a buffer. But the Systick timer goes crazy. i get way m...

yIzumi by Associate II
  • 3340 Views
  • 5 replies
  • 3 kudos

stm32c011

please let me know my coding is correct ,whether usage of my exti is correct  while (1) { HAL_Delay(300); // MAINS INPUT Adc_Mains(); HAL_ADC_Start(&hadc1); HAL_ADC_PollForConversion(&hadc1,1000); Main...

SRAM.11 by Associate III
  • 1138 Views
  • 0 replies
  • 0 kudos

Pwr_wakeup

I couldn't able wakeup the system after standby (wakeup should be switching ON mains ) the wakeup pin PA2 is connected to mains pin configured for pwr wakeup.  int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuratio...

SRAM.11 by Associate III
  • 1301 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H7 SPI vs STM32F4 spi

Im moving my project code from stmf407 to stm32h743 and i have stucked with spi. First of all stmh743 has many more registers and it also lack some of them like RXONLY register in CR1. What im trying to do its receive 19bytes from the master,the mast...

Screenshot_2.png stm32f4 init.png after_init_STmh7.png h7 clock.png

Where can I get the MB1671A microphone expansion board?

I have previously responded to #00152980 regarding TrulyHandsfree by Sensory.I recently purchased an STM32H747I-DISCO through Mouser.I tried to test it immediately but realized that I did not have the MB1671A microphone expansion board on hand.Where ...

TSuzu.2 by Associate
  • 1389 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.