STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USART2 problem

Hello,I would like to ask a question, I'm usin a STM32F429I-DISC1 REV-E01 for a TouchGFX application. I want to send data by UART to my pc. I configure CubeMX (screenshot attached) and then, in my code, I write those lines for a test. But it does'nt ...

ABIZO.1 by Associate II
  • 2384 Views
  • 2 replies
  • 0 kudos

FR_NOT_READY with SDIO, microSD 32GB and MCU STM32F407

I was trying to interface a microSD card (32GB) with STM32F407 through SDIO. Tried 1-bit and 4-bit modes. But it always gets me back FR_NOT_READY. and the program always stuck here: FATFS configuration: SDIO configuration: Clock:Where I'm doing any m...

MKDas_0-1691048899635.png MKDas_1-1691048968290.png MKDas_2-1691049050508.png MKDas_3-1691049071703.png
MKDas by Associate II
  • 1032 Views
  • 0 replies
  • 0 kudos

Resolved! GPIOC_CRL CNF2[1:0]

STM32F103RBHi. I tried to learn register level programming and got a problem with Port configuration register.hire is my codes:#include "stm32f1xx_hal.h"int main(void){RCC->APB2ENR |= RCC_APB2ENR_IOPCEN;GPIOC->CRL=0;GPIOC->CRL = GPIO_CRL_MODE2 | GPIO...

image.png
Gedo by Associate II
  • 2696 Views
  • 4 replies
  • 1 kudos

Resolved! STM32H725VGH6 interleaved mode

Hi! I am using STM32H725VGH6 series MCU, in the datasheet it is clearly mentioned that it has 2 direct 16bit ADC channels, while it is not there when trying to configure in STM32CubeIDE. Can you make sure the datasheet is correct or not?

shaktipg by Associate II
  • 4737 Views
  • 8 replies
  • 3 kudos

Resolved! clock voltage is 1.68 on nucleo-f413zh

hey everyone im using nucleo board f413zh for an audio project and i have a weird clock voltage of 1.68 when i enable master clock  , the clock signal came from the st link to the mcu i have 2 board and in the two is the same problem  i check vdd and...

Screenshot (263).png Screenshot (262).png
zohbou1 by Associate
  • 2626 Views
  • 4 replies
  • 0 kudos

Resolved! STM32H563 LSCO

Just getting started with this MCU. STM32CubeIDE says LSCO has conflict with GPIO input on PB2. Using this IDE how do I disable LSCO?

Clicker2 Clock Config (Newbie Errors I'm Sure)

Greetings, I have purchased a Clicker2 from MikroElectronica mainly because it has the facility to host their Click Boards ecosystem while working with the STM32CubeIDE. I can't say that I am a fan of their abstracted SDKs and code that is too dissim...

CoachTacamo_0-1690301098868.png

stm32l053r8 smbus

hi,my self Revanth im using bq40z50 which Supports Two-Wire SMBus v1.1 i want to integrate this with stm32l053r8 in the data sheet it was mentiond as it will support for smbus 2.0 so will it support for smbus v1.1 as well ??? can anyone help me with ...

Stm32f105 SPI3 change pins

I am running a simple poc to test the SPI connection to a flash memory chip. When I select SPI3 in cube MX, It gives me two options for the set of pins. I would like to use PC12 as Clock but it wont let me change it. Hand editing the generated code d...

coolname by Associate II
  • 1722 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.