2023-08-03 5:41 AM
I couldn't able wakeup the system after standby (wakeup should be switching ON mains ) the wakeup pin PA2 is connected to mains pin configured for pwr wakeup.
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_ADC1_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
/* Enable Power Control clock */
__HAL_RCC_PWR_CLK_ENABLE();
/* Check if the system was resumed from Standby mode */
if (__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET)
{
/* Clear Standby flag */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
/* Check and Clear the Wakeup flag */
if (__HAL_PWR_GET_FLAG(PWR_FLAG_WUF4) != RESET)
{
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF4);
}
}
while(Mains<0.1)
{
count++;
if(count>=30)
{
HAL_PWR_EnterSTANDBYMode();
}
else
{
count=0;
}
}
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN4_HIGH);
while (1)
{
HAL_Delay(100);
// MAINS INPUT
Adc_Mains();
HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc1,1000);
Mains=HAL_ADC_GetValue(&hadc1);
Mains=Mains*2/4095;
HAL_ADC_Stop(&hadc1);
HAL_Delay(100);
//Battery operation
Adc_Vbat();
HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc1,1000);
Vbat=HAL_ADC_GetValue(&hadc1);
Vbat=Vbat*2/4095;
HAL_ADC_Stop(&hadc1);
HAL_Delay(100);
//OPEN CIRCUIT DETECT
Adc_OCD();
HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc1,1000);
OCD=HAL_ADC_GetValue(&hadc1);
OCD=OCD*2/4095;
HAL_ADC_Stop(&hadc1);
HAL_Delay(100);
//BATTERY TEMPARATURE
Adc_Temp();
HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc1,1000);
Temp=HAL_ADC_GetValue(&hadc1);
Temp=Temp*2/4095;
HAL_ADC_Stop(&hadc1);
HAL_Delay(100);
// Check mains and mains fail
if(Mains>0.1)
{
if((Mains<1) &&(Vbat>0.9))
{
En_Emergency(1);
Set_LED(0);
}
else
{
En_Emergency(0);
}
}
// MAINS ON
if(Mains>1.2)
{
if(Vbat>1.5 || Vbat<0.5) //OPEN CIRCUIT OR ZERO BATT LEVEL
{
Set_LED(0);
Batt_Chrge(1);
}
else if(Vbat <0.94 ) // START CHARGING LEVEL
{
Set_LED(1);
Batt_Chrge(1);
}
else if(Vbat >0.98 ) // STOP CHARGING LEVEL
{
Set_LED(1);
Batt_Chrge(0);
}
//BATTERY TEMPARATURE CHECK
if(Temp<0.17 || Temp>0.83)
{
Batt_Chrge(0);
Triple_Flash();
}
else if((Temp>0.17 || Temp<0.83))
{
Batt_Chrge(1);
}
}
2023-08-03 6:24 AM - edited 2023-08-03 6:26 AM
If Mains is initialized to 0, which as a global variable presumably it is, your code will never get out of this loop and thus will never enter the main loop.
while(Mains<0.1)
{
count++;
if(count>=30)
{
HAL_PWR_EnterSTANDBYMode();
}
else
{
count=0;
}
}
2023-08-03 7:45 AM
can you please help me to solve.
if(Mains<1)
{
count++;
if(count>=300);
{
HAL_PWREx_EnterSHUTDOWNMode();
}
}
i tried this too but the problem is in wakeup
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.