STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to use ST32MC0 for I2C communication over 2050 bytes?

I am using STM32C031C6 for I2C verification.I tried to communicate 2050 bytes of data using the HAL driver.However, it did not receive the correct data.To be precise, the data at 512,1024,1344,1346,1538,18561 and 1858 bytes were different.The setting...

kkazu by Associate II
  • 3806 Views
  • 4 replies
  • 1 kudos

Resolved! [STM32L431] BORRSTF always SET after powering up

Hello,I want to read the BORRSTF value to detect the previous reset situation during the start process. but BORRSTF always reports '1'.BORRSTF can be clear with RMVF, but there is a problem that makes it impossible to tell whether it is an initial st...

000001.PNG 00002.PNG 00004.PNG

stm32h7 fmc lcd 8 bit setup

I've been trying to run the fmc and lcd over an 8-bit data line for a few days. Yesterday I managed to read the ids of the lcd correctly, but because I messed up the timing settings of the fmc (timing settings were working randomly), I can't get any ...

combine_images.jpg ss4.png ss5.png

STM32H7 ADC3 over BDMA only writing to buffer once

I am working with a STM32H723 micro, capturing 2048 samples of data on ADC3. The ADC is triggered by the overflow of TIM1 and transfers samples successfully the first time HAL_ADC_Start_DMA(&hadc3, (uint32_t*)adc_buf, ADC_BUF_LEN); is called.In the H...

Iris-DM by Associate III
  • 4923 Views
  • 6 replies
  • 0 kudos

Resolved! Can't start MCU on Nucleo-H563ZI when powering through E5V

I have Nucleo-H563ZI board and I'm trying to power it through external 5V source (E5V). When I connect the 5V power source and set PWR SEL jumper (JP2) to E5V, I can see the power LED (LD5) light up and even the ethernet controller seems to be active...

continuum by Associate II
  • 4426 Views
  • 6 replies
  • 2 kudos

Resolved! STM32F769I-DISCO

Hello.I am developing a product with STM32F769I-DISCO development kit.Unfortunately, by my mistake, I think I connected 24VDC to the power terminal, so I couldn't use the power IC that looked like a regulator marked U4.Can you check the exact name of...

R3D3 by Associate II
  • 4153 Views
  • 4 replies
  • 4 kudos

Power Wake UP

Hi,Im using stm32h7 mcu for my project.Which is an iot product.I need to use low power mode on it  i need to wake the mcu using an gpio external interrupt or either by an uart .Device is switch to some mode with a constant current consumption which i...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.