STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB1.0

Hi,I using Eval boar : stm3210E-eval (stm32F103ZG6)I want to communicate with an external device vua USB, this device should be communicatre with USB1 gen,I ask if it could be with this eval board?>If not, if I use this MCU stm32f103ZG6 and make a pr...

HT by Associate
  • 1472 Views
  • 1 replies
  • 0 kudos

Resolved! EXTI only exits STOP Mode 2 the first time

Hello,I have a test app that starts in wake for 5s (with "high" current and GPIO output high) then enters STOP Mode 2 (with "low" current and GPIO output low). It remains in that mode until the EXTI 1 interrupt is triggered by a button press, which w...

EC.3 by Associate III
  • 4060 Views
  • 3 replies
  • 0 kudos

TIMERS SYNCHRONIZATION DOES NOT WORK

hello everyone im working with stm32f4 nucloe board , i want to implement one wire communication to send data to a microphone but also i need a clock above 40khz to send this data for that im using two timer in master slave mode , one for generating ...

zohbou by Associate
  • 3631 Views
  • 0 replies
  • 0 kudos

stm32U585 FMAC IIR wrong result

Hi.I have a big buffer with Chirp data for testing that about 30000 of int16 length and I can not get right result from FMAC IIR filtering operation. The operation configured in polling for read and write.I calculate a bandpass IIR DF1 filter coeff w...

MehranMsba_0-1694019611137.png MehranMsba_1-1694019697889.png

Resolved! STM32L476VCT6 VREF connection

Hello!In my project I'm using STM32L476VCT6. I don't want to connect external voltage reference, only internal. Could I leave floating pins VREF- and VREF +?  I saw in the datasheet that these pins could be tied internally to Vdda and Vssa correspond...

Resolved! stm32u5 vdda abnormal current consumption

I set several unused pins in stm32u5 to floating as hardware and set them to low output by pushpull for ESD protection.The microcontroller was heating up abnormally when I looked at it with a thermo camera, and I found that the current consumption of...

Resolved! Strange in debugging NOR Flash

In STM32CubeIDE, the NOR Flash seems to work fine that data was correct both by reading to variable and reading 0x90000000 of memory mapping address.But if terminate the session and restart and just read the data, it is all gone.And there is another ...

Charles_Li_2-1693971120181.png Charles_Li_3-1693971306706.png

Issue with STM32 USB Transmit Interrupted by Receive

Posted on August 11, 2015 at 07:05The Scenario: I have a custom board running an STM32F303VCTx connected via USB (Full Speed Device) to a Linux machine as a Custom HID peripheral.  A majority of the time the system works correctly sending data in bo...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.