2023-09-07 10:03 AM
hello everyone
im working with stm32f4 nucloe board , i want to implement one wire communication to send data to a microphone but also i need a clock above 40khz to send this data for that im using two timer in master slave mode , one for generating the clock and one for one wire communication , for the one wire communication im creating a delay with the slave timer and set/reset the gpio pin , the weird thing is when the clock of master is above 2khz the one wire communication doesn't work i dont know what it happen i dont if someone can guide trough this thanks
int main(void)
{
/* USER CODE BEGIN 1 */
HAL_TIM_Base_Start(&htim1);
char spi_buf[SAMPLES];
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USB_DEVICE_Init();
MX_CRC_Init();
MX_TIM1_Init();
MX_TIM8_Init();
MX_TIM2_Init();
/* USER CODE BEGIN 2 */
TimerDelay_Init();
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);
HAL_TIM_PWM_Start(&htim8, TIM_CHANNEL_1);
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);
//HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_1);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
// Start the I2S DMA receive
// HAL_I2S_Receive_DMA(&hi2s1, (uint16_t *)spi_buf, SAMPLES);
// Wait for the DMA receive to complete
// Now, you can transmit data
sapce();
transmit_start_pilot();
sapce();
// Transmit data bits
for (int i = 0; i < sizeof(sequence) / sizeof(sequence[0]); i++) {
onewire_write_bit(sequence[i]);
}
sapce();
// Transmit stop signal
transmit_stop();
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.