STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Nucleo l010RB weird label and strange spi behavior

Hi,I buy a new board L010RB, but it is labelled with classic strap "NUCLEO-L010RB" but there is one line after with is "NUL010RB$AU2". I had a couple of L010RB before but it's the first time i have such label on it.I'm wondering what is mean.Plus I'm...

IMG_20230906_082403.jpg
JAgue.1 by Associate II
  • 1920 Views
  • 3 replies
  • 0 kudos

Riverdi (display) connection with external PHY

Hello. I have a RIVERDI display with the STM32H757XIH6 (2MB Flash, 1MB RAM) microcontroller. I am trying to develop for this display a program  in order to connect it with an external PHY. In my research for external PHY I have found the LAN8720. Alt...

Resolved! STM32G030 BOOT0 versus SWD

STM32G030 datasheet indicates BOOT0 is PA14-BOOT0 and that SWDIO is PA13 and SWDCLK is PA14-BOOT0.Upon power up, how does the STM32G030 know whether PA14-BOOT0 is controlling whether to enter bootloader mode or is SWDCLK?Since STM32G030 has no JTAG c...

STWIN.box Virtual COM Port under Ports (COM & LPT)

Dear STM32U585AIIXQ Community,I recently acquired an STWIN.box development board and have been attempting to establish a communication link with my computer via the USB interface. Unfortunately, my computer is not recognizing the COM port associated ...

AkaPaDa_18_0-1694532637614.png

Resolved! serial.peek() and serial.flush() equivalent in STM32

I'm trying to port a UART driver from aurdino to STM32. Able to relate all interfaces for aurdino vs STM32 while can't able to map ones for the followingserial.peek()serial.flush()Does HAL have an direct interface as peek() to get the next byte of in...

darthana by Associate
  • 7503 Views
  • 5 replies
  • 1 kudos

TICK_INT_PRIORITY changes from 0 to 15 and vice-versa

STM32CubeIDE - Version: 2.0.200.202301271415STM32CubeMX - Version: 6.8.1-RC4  Build: 20230419-1431 (UTC)I just added two DMA channels to UART1 and noticed a change in stm32h7xx_hal_conf.h The project uses LwIP and FreeRTOS. FreeRTOS relies on TIM6 as...

PriorityChanged.png
ARaid.1 by Associate III
  • 6182 Views
  • 6 replies
  • 0 kudos

I2C sensor on USART 2 Serial communication

Hello, I am using the embedded coder support package in simulink to interface with my onboard MEMS acceleration sensor (LSM303AGR) on my STM32F411VET discovery board. I could successfully connect and run simple LED program through USART2 on simulink ...

Resolved! Schematic of NUCLEO Board missing

Hi, I have bought a NUCLEO-F756ZG board to explore the F7 controller.I need the schematic to work with it. In the manual:https://www.st.com/resource/en/user_manual/um1974-stm32-nucleo144-boards-mb1137-stmicroelectronics.pdfThere is only a note on pag...

Moritz1 by Associate III
  • 3915 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.