STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Multiplexed OCTOSPI in STM32H7B0RBT6

Hi,I would like to know if it is possible to have the mutiplexed octospi in the microcontroller stm32h7b0rt6 as it mentionned in AN5050 in Figure 11cause when I tried to configure it using the CubeMx the CS pin for OCTOSPI2 is not found as it is mand...

ALAMI_Othmane_0-1694625578777.png ALAMI_Othmane_1-1694625761689.png

Resolved! MCU shutting down during SPI communicaiton

I have a simple demo board with a STM32L451VET6, a SPI LCD and four switches. The board will send the first byte over SPI perfectly, then either during or right after sending the second byte - it appears the MCU shuts down - as the CS line drifts dow...

Stoufer_0-1694538436110.png
Stoufer by Associate III
  • 6969 Views
  • 11 replies
  • 0 kudos

Resolved! More SPI trouble !

Hey Guys - more SPI issues!I have a new board with minimal connections - basically just SPI to a LCD and four pushbuttons. I created a new STM32 project in STM32cube.It is using a STM32F451VET6 with clock set to MSI RC 4000kHzI configured SPI in the ...

Stoufer_0-1694467500960.png
Stoufer by Associate III
  • 2537 Views
  • 4 replies
  • 0 kudos

CycloneSSL

Hello everyone,I'm trying to do signing and verification using ECDSA on stm32 boards with the CycloneCrypto library. As it's only for evaluation at the moment, I'm not looking to build the whole project. So, would there simply be directories where th...

Resolved! UART bootloader

Hello! I'm utilizing the STM32L476VCT6 in my project. Through the UART (PC4, PC5), this MCU interfaces with the Wi-Fi SoC. For firmware updates, I want to use this UART connectivity. But I notice that USART3 bootloader has dedicated PC10, PC11 pins. ...

Resolved! STLINK-V3MINIE errors on programming STM32G071

Using both STM32CubeIDE and STM32CubeProgrammer; both fail to successfully program using the STLINK-V3MINIE. The part is IDs correctly and "Full chip erase" works without errors. I only get an error once I click the "Start Programming" button. Same b...

natan by Associate
  • 3608 Views
  • 3 replies
  • 0 kudos

Resolved! Riverdi diplay with STM32H7 and external PHY.

Hello! I would like to know if I could connect my riverdi screen through expansion connector that provides with the external PHY LAN8720, or the only way is by PoE of riverdi. Can anyone provide some information about this? The datasheet of the scree...

Resolved! LCD parallel Interface vs LCD TFT Controller

I have an 8 bit parallel, 240x280 TFT display and was wondering:What's the difference between the "LCD parallel Interface" and the "LCD TFT Controller" under the "Display controller" section?Is there a significant difference in fps or processing cons...

btorres_0-1694569952724.png
btorres by Associate II
  • 13827 Views
  • 8 replies
  • 4 kudos

ADC results randomly sorted

Hi Iam using STM32F407 discovery board and iam trying to sample 8channels of an ADC. Iam trigerring the ADC with a timer and Iam also using DMA whitch interups the code when the DMA buffer is full. Timer freq is 12kHz. DMA is in circular mode.Problem...

Chochy_0-1694615211925.png Chochy_1-1694615224140.png Chochy_2-1694615232630.png Chochy_3-1694615313356.png
Chochy by Associate
  • 3275 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.