STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ADC Sample Rate

I am doing current control with PWM. The switch provides a current sense pin which is going to my ADC.I am using STM32F4. I am also using FreeRTOS, not sure if this is important though.My ADC is set to run at 84MHz with 4x prescaler. The conversion i...

TonyFauci by Associate II
  • 4596 Views
  • 5 replies
  • 0 kudos

Facing issues with interrupts

Hi,I face some issue with the interrupts of STM32L452RET6P. I have two codes running in the controller one is a custom bootloader code and other is an application code which stored in flash memory. when the device get reset it will run the custom boo...

SSaiy.1 by Associate III
  • 3262 Views
  • 5 replies
  • 1 kudos

Library FingerPrinter for STM32 blue pill

HELLOI need to use a biometric sensor with stm32 blue pill (stm32f103c8t6) and I am looking for a library to use with the CubeIde software, does anyone have libraries for it?Thanks

robert456 by Associate II
  • 3772 Views
  • 6 replies
  • 0 kudos

Resolved! STM32H757 Ethernet communication not working

Hello ST TeamI am working on medical project involving patient monitoringCurrently we are using the STM32H757XI-EVAL board and trying communicate the host monitor via ethernet TCP/UDP. The underlying operating system is Azure RTOS.I am not able to fi...

Lokesh1 by Associate II
  • 3904 Views
  • 4 replies
  • 0 kudos

Resolved! How to edit RTC Alarm parameters

Hi, I use RTC alarm to wake up from STOP mode I have STM32F030C8T6. During initialization I have set 5s and everything works as it should. But I would need to change the interval to maybe 30s while the program is running. The problem is that the chan...

DJeze.1 by Associate II
  • 9757 Views
  • 2 replies
  • 0 kudos

Resolved! Nucleo STM32U575ZI-Q low level USART receiving help

Hi all,I am using the Nucleo STM32U575ZI-Q and have been trying to get low level USART with DMA working. Transmitting data works fine as I can see the data using a logic analyser but when I try to receive data either from another Nucleo or putting th...

JNoon.1 by Associate III
  • 4990 Views
  • 4 replies
  • 1 kudos

SPI TRANSMIT ON STM32

Posted on March 10, 2016 at 11:19 I am using a custom made STM32F302RE board. I have configured my SPI as follows: hspi2.Instance = SPI2; hspi2.Init.Mode = SPI_MODE_MASTER; hspi2.Init.Direction = SPI_DIRECTION_2LINES; hspi2.Ini...

akshayamk by Associate II
  • 1466 Views
  • 1 replies
  • 0 kudos

Resolved! How to check HSE has stop

I am using STM32H7A3/7B3 to my project.Currently I use HSE as for the system clock.There is a process when press power OFF MCU will go to STOP mode.My question how to check that HSE has stop and enter the STOP mode correctly?

NRAML.1 by Associate II
  • 2500 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.