STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to settings HRTIM and TIM1 is synchronized

Hi.I use the STM32G474.To start TIM1 synchronized with HRTIM, I will use "hrtim_out_sync".I have a question.If I use "hrtim_out_sync", Can I start TIM1 at same time and reset ?I want to set a same frequency for HRTIM and TIM1 and start simultaneously...

smiya.2 by Associate II
  • 6258 Views
  • 2 replies
  • 1 kudos

Resolved! Why no High Speed USB for STM32H5?

The STM32U5 has HS PHY and it's slower than the STM32H5 so why doesn't the H5 have HS PHY or any HS USB support? Will a version that does be released in future? Its almost the perfect chip to use for a future project I have in mind aside from the lac...

etheory by Senior II
  • 4408 Views
  • 1 replies
  • 0 kudos

warning

Description Resource Path Location TypeProject 'somno_touch_sd' has no explicit encoding set somno_touch_sd /somno_touch_sd No explicit project encoding 

benedito by Associate
  • 6671 Views
  • 1 replies
  • 6 kudos

Resolved! MCU Programmer Adaptor

I am using STM32F302R6T6 MCU. I'm making a board. I will communicate with the MCUs via the I2C protocol. I am designing a card with a Master-Slave structure. Can I program the MCU if I add SDA, SCL, +5V, and GND pins to the board and connect them to ...

bngstskn by Associate III
  • 5936 Views
  • 4 replies
  • 2 kudos

STM32H743 general VLAN handling not working as described

I am currently implementing a Profinet protocol on the STM32H743 which needs VLAN information in some packet types. Since the VLAN tags are already generated by the software for transmit packets I tried to get these tags passed through the Ethernet M...

JMH by Associate II
  • 4981 Views
  • 2 replies
  • 2 kudos

Resolved! Nucleo-H755ZI-Q not detected by usb

Hi thereI bought two Nucleo-H755ZI-Q (NUH755ZIQ$AT3) boards.Non of them show up as USB devices on either of my computers.I have tried connecting through the IDE 1.13.1; STLinkUpgrade  3.12.3 and the newest cubeprogrammer. neither can find the device....

JOKH by Associate
  • 6438 Views
  • 3 replies
  • 2 kudos

STM32H745 LTDC Interface

Dear STM community,We are using a STM32H745 microcontroller interface with 1280 x800 TFT lvds display.RGB data from controller LTDC data convert through SN75LVDS83 ic and LVDS data fed to tft display.we are facing a issue in pixel format which is not...

D6 by Associate
  • 2366 Views
  • 1 replies
  • 0 kudos

STM32 with usb HUB and multiple STM32 devices

Hi,I been trying to set up a stm32F405 mcu usb host with a hub onto which 4x stm32 device is connected. I would use these 4 devices to send data to the main mcu periodicaly at 50Hz, and to have the data transfer syncronised from the 4 devices to be o...

RBacs.1 by Associate II
  • 15755 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.