STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SDMMC does not work after power cycle

Hi,I am using STM32H747. I have successfully write&read micro sd card over SDMMC2 peripheral while debugging. But after debugging, when I power cycle or reset the board, I am not able to use sd card. I see FatFS open file failing. The board is arduin...

serhat1 by Associate
  • 4023 Views
  • 1 replies
  • 0 kudos

How to use printf/scanf in both cores using SWO?

I have the M7 core running and printing debug messages to the IAR Workbench terminal, and also have the M4 doing something similar. My probem is that I get a hard fault in the M4 core if the its printtf messages are included in the build. If I don...

Resolved! PWM Dim

I am trying a PWM output with jumper connectors.when mains fail(input supply)PWM is on indicated by a lamp and OFF when there is a supply .in between if the supply is OFF and Lamp is in ON there is a jumper connect to PA6 (input)of stm32c011f6p6.if t...

SRAM.11 by Associate III
  • 4722 Views
  • 3 replies
  • 0 kudos

STM32L031 Programming and debugging using Tag Connect

Hello. I am currently working with the STM32L031 Nucleo board:https://www.st.com/resource/en/user_manual/um1956-stm32-nucleo32-boards-mb1180-stmicroelectronics.pdf The board has integrated ST-LINK so it is quite easy and convenient to flash the devic...

tag_connect.png
LPetr.1 by Senior II
  • 8491 Views
  • 5 replies
  • 0 kudos

Does powering shorted board hurt stm32?

firstly i am new to here, dont know much rules about posting. 1 minute ago i saw post about shorted power dont kills mcu but can it damage stm32?so i shorted my 3d printer board(stm32g0b1ret6 probably) via 3.3v and gnd(general probably). i checked by...

Hoorow by Associate II
  • 9606 Views
  • 10 replies
  • 3 kudos

Unstable voltage supply to STM32U

Hello all, I have designed a board for sensing purposes and I am using the following ST components: STM32U575ZIT6Q. I am supplying this component with 3V3, which I get form a 5V/3V3 LDO. Between the output of the LDO and the supplying rail to the STM...

MicrosoftTeams-image (5).png MicrosoftTeams-image (6).png STM32_Schematic.JPG
KKots.1 by Associate II
  • 5601 Views
  • 7 replies
  • 2 kudos

Resolved! STM32F103 input timer interrupts...

I have a test project that sets up TIM3.3 to count microseconds between falling edges of the timer input.  The timer is started with a call to HAL_TIM_IC_Start_IT(&htim3, TIM_CHANNEL_3); to start timing the input.  Inside HAL_TIM_IC_CaptureCallback(*...

DBudd.1 by Associate II
  • 4269 Views
  • 5 replies
  • 1 kudos

Resolved! STM32L0 LPUART LSE Error

Hello everyone,I'm working on a project with a STM32L072CBT6.I'm using LPUART (PB10 / PB11) at 9600 bauds to communicate with an other board. For low power consumption, i'm using LSE for my LPUART.When i check my bauds rate on my oscilloscope, i get ...

MLam_0-1694707277000.png MLam_1-1694707448466.png MLam_2-1694707527865.png MLam_3-1694707578320.png
MLam by Associate III
  • 4579 Views
  • 7 replies
  • 1 kudos

How to shorten wakeup time from STOP mode

Hello,Is there any specific guidance regarding how to improve wakeup time from the various STOP modes? The U5 Reference Manual mentions that configuring STOPWUCK = 0 will use the MSIS up to 24 MHz, which would be faster than HSI16. I've used that alr...

EC.3 by Associate III
  • 7333 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.