2023-09-18 4:33 AM
Hi there
I bought two Nucleo-H755ZI-Q (NUH755ZIQ$AT3) boards.
Non of them show up as USB devices on either of my computers.
I have tried connecting through the IDE 1.13.1; STLinkUpgrade 3.12.3 and the newest cubeprogrammer. neither can find the device.
I suspected driver issue and reinstalled the en.stsw-link009 driver
Still no luck; also the devices are not shown as "unknown" there is no reaction at all from the PC when i plug and unplug the device.
The MCU is running the preprogrammed program that switches between LD1,2 and 3 when user button is pressed. but except from that; nothing is working.
They also do not show up as
Solved! Go to Solution.
2023-09-18 5:19 AM
Are you using the CN1 USB connector?
Perhaps try a different USB cable, could be using a power-only cable.
2023-09-18 4:35 AM
2023-09-18 5:19 AM
Are you using the CN1 USB connector?
Perhaps try a different USB cable, could be using a power-only cable.
2023-09-19 4:32 AM
I did use the CN1 but the two cables I tried were apparently power-only cables.
I guess third time really is the charm.
Thank you for your response.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.