2023-09-18 10:40 PM
I am using STM32F302R6T6 MCU. I'm making a board. I will communicate with the MCUs via the I2C protocol. I am designing a card with a Master-Slave structure. Can I program the MCU if I add SDA, SCL, +5V, and GND pins to the board and connect them to the relevant pins of the MCU? Is it a problem? Or do I need to purchase a Programmer Adapter? The programmer adapter is not useful as I will be coding a lot of boards. And I use an NTC sensor. I will also add the necessary pins for the NTC sensor.
Solved! Go to Solution.
2023-09-19 5:31 AM
Programming over SWD using a supported programming adapter such as STLINK-V3MINIE is the best method. You can also use the bootloader as described in AN2606, but will have limited insight into the chip should debugging be necessary.
2023-09-18 10:51 PM
And additionally I will add the necessary ST-link pins to connect the computer
2023-09-18 11:01 PM
Hello bngstskn
I have found the following tutorial:
https://www.st.com/resource/en/application_note/an4045-stm32f3-series-inapplication-programming-iap-using-the-usart-stmicroelectronics.pdf
However, in the reference manual from your MCU there is the following remark (under 4.2.3): "In contrast to the ICP method, the In-Application Programming (IAP) can use any
communication interface supported by the microcontroller (I/Os, USB, CAN, UART, I2C, SPI, etc.) to load programming data into memory. IAP allows the user to reprogram the flash memory while the application is running. However, part of the application must have been previously programmed into flash memory using ICP."
I would say you still need an ICP, such as an ST-LINK/V2. You could build an adapter and put your favorite connector for it on the board. I take for example this connector and made an adapter for it. With it you are very fast in programming.
https://www.reichelt.de/ch/de/jst-stiftleiste-gerade-1x5-polig-xh-jst-xh5p-st-p185076.html?&nbc=1
Greetings Touby
2023-09-18 11:08 PM
Hi Touby,
I will take into account what you say,
Thank you.
2023-09-19 5:31 AM
Programming over SWD using a supported programming adapter such as STLINK-V3MINIE is the best method. You can also use the bootloader as described in AN2606, but will have limited insight into the chip should debugging be necessary.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.