STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

''unknown device'' error in ST Link Utility

Posted on November 27, 2015 at 10:52When I try to target->connect in ST Link Utility I have an error ''unknown device'' with disco L4, disco F7 and nucleo L4. With nucleo L0, the connection is good, but I have the message ''Device family : unknown d...

SPI Clock rate limitation?

TL;DR. What are the limiting factors for incoming clock speed for an SPI peripheral operating in slave mode?I'm using the STM32U575 MCU with a few peripherals, and am clocking it down to 16MHz for SYSCLK and all related peripherals.  I'm generating a...

sethkaz by Associate III
  • 13780 Views
  • 15 replies
  • 3 kudos

Using SPI to interface to TI ADC & DAC

hi, i m a student learning STM32 for the first time, my project now is to interface stm32h7 using SPI to TI ADC TLV1570 and DAC TLV5608. Anyone has tutorial and any reading material on this to share? thanks in advance. 

Can i manage this device from windows 10?

Hi i have this devicehttps://es.aliexpress.com/item/1005003425526257.html?spm=a2g0o.order_list.order_list_main.29.21ef194dpi5ufM&gatewayAdapt=glo2espSomeone can give me some info about how to access it from windows 10?thanks very much in advance.

ptt by Associate II
  • 12507 Views
  • 16 replies
  • 2 kudos

STM32L496GT6 battery voltage monitoring

I want to monitor battery voltage (Vbat). I use the adc function to monitor voltage on the Vbat pin, and it can't read the voltage. When I use the same function on other pins, it can read correctly. For Vbat monitoring, what are the specific configur...

JThas.1 by Associate II
  • 2010 Views
  • 3 replies
  • 0 kudos

Resolved! Lan8742 Hardfault

Stats:STM32CubeIDEVersion: 1.13.2Build: 18220_20230914_1601 (UTC) Windows 10 Enterprise I have a project using STM32H743 and Azure RTOS, ThreadX, NetX, and FileX.In the NetX portion during initialization of the netx thread, the code performs initiati...

GreenGuy_0-1695862962474.png GreenGuy_1-1695863168854.png

LoRa example for STM32WL | un able to read from UART

I am currently working on the LoRaWAN_END_NODE example project for a stm32WL . And I want to receive external data via uart and use the LoRaWan process continually, however I am getting problems. I am unable to read from the UART the second time I ca...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.