STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! 32kB flash overflowing using just USB CDC and SPI

Hello everyone,I am trying to use both USB CDC and SPI on a STM32F042F6P6 MCU. Unfortunately, without even writing almost any code (just an HAL_SPI_TransmitReceive() and a CDC_Transmit_FS()) it says the flash memory overflows by 1484 bytes.Is this no...

LLope.31 by Associate III
  • 2784 Views
  • 2 replies
  • 1 kudos

STM32CubeIDE not flashing MCU

Hi! I'm trying to flash a STM32L422KBT6 with STM32CubeIDE 1.13.2 and ST-LINK V2 and I keep getting this error: Error: failed to erase memoryEncountered Error when opening C:\ST\STM32CubeIDE_1.13.2\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externa...

Resolved! SystemClock_Config() fails with some clock rates

I'm trying a simple blinking LED on a STM32H743VIT6 with STM32CubeIDE 1.13.2, using the clock configuration wizard. When the clock rate is set to 90MHz everything is fine, but at 480MHz the program cannot get past the SystemClock_Config() call. When ...

iforce2d by Associate III
  • 2565 Views
  • 3 replies
  • 1 kudos

STM32F103RCT6 - BusFault on address 0x20010000

Hi all,I'm trying to debug a bus fault that happen on a region on ram that is not supposed to exists. MCU has 48kb of RAM, so start from 0x20000000 to 0x2000C000, but i'm able to write 0xFF from 0x2000C000 to 0x20010000.. why??I can see also some dat...

rdzdvd_0-1696414700487.png
rdzdvd by Associate II
  • 4878 Views
  • 4 replies
  • 0 kudos

System bootloader

Hello,I'm currently working on a system bootloader using an STM32L4P5VGTx board. During this process, the board entered an unknown state and doesn't seem to recover even after a reset.I also attempted to use the Cube Programmer tool to load a bin fil...

pvall.1 by Associate II
  • 1253 Views
  • 1 replies
  • 0 kudos

Not expected frequency on NUCLEO-L496 RTC output calibration

Hi,I'm trying to improve the accuracy of RTC. For that, I use the AN2604 witch describe this.But, when I activate the calibration output of RTC at 512Hz, I have only 496Hz at the output. (AsynchPrediv =127). I tried this simple code to the nucleo-L47...

Sirac by Associate III
  • 4034 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.