STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Excluding DMA from Scatter File CCM memory section

Hi, I have created scatter file: ; ************************************************************* ; *** Scatter-Loading Description File for STM32F4 *** ; ************************************************************* LR_IROM1 0x08004000 0x00...

JBond.1 by Senior II
  • 1607 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F44: UART Noise/Frame error with externel CPU clock

HiI have a self designed board (STM32F44 MCU) with an UART communication. It works well as long as I configure it to use the internal clock. As soon as I switch to the external clock (oscillator), the UART communication gives a noise and frame error ...

Corono_0-1696607734866.png
Corono by Associate III
  • 4048 Views
  • 5 replies
  • 0 kudos

Resolved! STM32H7 | MPUs in dual cores

Hello @ all,I'm dealing with a project with stm32H755 MCU, as you know it is made of two cores: cortex-M7 and cortex-M4. Keeping in mind I'm using a few peripherals, among which FDCAN, SPI and most importantly lwIP/ETH, I'm trying to put together all...

Zzaaack by Associate III
  • 3455 Views
  • 3 replies
  • 3 kudos

HAL_TIM_Base_Start_DMA - STM32CubeMX

Posted on September 14, 2016 at 12:27I've try to use HAL_TIM_Base_Start_DMA with TIM6.To configure the system I'm using STM32CubeMX. We I start the project I can't receive any interrupt...HELP.In Attachment the ioc file.My change after code generati...

Resolved! Maximum External Clock supported by stm32F767.

I looked at both the datasheet and Oscillators design document for stm32 controllers. Both suggested the same speed for external Osciallaotrs for stm32F7 controllers that is 4-26 MHz.BUT, in the stm32cubeMx it gives you option to select external HSE ...

CJami_0-1696839447346.png CJami_1-1696839455028.png CJami_2-1696839494005.png
CJami by Associate III
  • 3169 Views
  • 4 replies
  • 3 kudos

Resolved! STM32F4 can I join SRAM and SRAM2 memories?

Hi, I have STM32F407VET6 which has such memory layout.Can I join SRAM (0x2000 0000 - 0x2001 BFFF) and SRAM2 (0x2001 C000 - 0x2001 FFFF) memories to one?Or do I must to manage them separately?

0693W00000YA0E4QAL.png 0693W00000Y8qzIQAR.png 0693W00000Y8qzDQAR.png
JBond.1 by Senior II
  • 2882 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.