2023-10-08 2:33 PM
Hi, I have created scatter file:
; *************************************************************
; *** Scatter-Loading Description File for STM32F4 ***
; *************************************************************
LR_IROM1 0x08004000 0x0007C000 { ; load region size_region
ER_IROM1 0x08004000 0x0007C000 { ; load address = execution address
*.o (RESET, +First)
*(InRoot$$Sections)
.ANY (+RO)
.ANY (+XO)
}
RW_IRAM1 0x20000000 0x0001C000 { ; RW data
.ANY (SRAM)
;.ANY (+RW +ZI)
}
RW_IRAM2 0x2001C000 0x00004000 {
.ANY (SRAM2)
;.ANY (+RW +ZI)
}
RW_IRAM3 0x10000000 0x00010000 { ; CCM data
.ANY (+RW +ZI)
.ANY (CCM_DATA)
startup_stm32f407xx.o (STACK)
startup_stm32f407xx.o (HEAP)
}
}
And added all DMA used buffers to SRAM section:
static uint8_t Buffer[BUFFER_SIZE] __attribute__ ((section("SRAM")));
The issue is if SRAM fills with other buffers, some buffers are moved to CCM section as they fall under this category ".ANY (+RW +ZI)". How to exclude SRAM sections from ".ANY (+RW +ZI)"? Whats the syntax to say ".ANY (+RW +ZI) - but not SRAM"?
Solved! Go to Solution.
2023-10-09 6:47 AM
Seems that defining ".ANY (.bss) .ANY (.data)" instead of ".ANY (+RW +ZI)" excludes "SRAM"
2023-10-09 6:47 AM
Seems that defining ".ANY (.bss) .ANY (.data)" instead of ".ANY (+RW +ZI)" excludes "SRAM"
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.