STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U575 change PWM output duty realtime

I tried to change PWM output duty without stopping or suspending PWM output, but between two times of writing new value to CCR, there must be a delay time inserted in. Following is the example code:/* if delay_ms(300), code can run correctly, if chan...

Using the FMC of the STM32U575 for SDRAM

Hello everyone,I am currently working with a STM32U575ZIT6 and am trying to connect as much RAM as possible to its FMC peripheral. However, SRAM and PSRAM are not available in the sizes I am looking for, so I was wondering if it would be possible to ...

PKolo.1 by Associate II
  • 1708 Views
  • 1 replies
  • 0 kudos

1. SPI communication between MCU and MPU.

Hi,I am working on SPI bus communication between IMX6dl MPU and STM32L476 MCU.MPU work as a master device and MCU work as a slave device.Configuration of MPU is:pinctrl_ecspi3: ecspi3grp {               fsl,pins = <                       MX6QDL_PAD_D...

SPare.9 by Associate II
  • 4348 Views
  • 6 replies
  • 0 kudos

Fan Out of single SPI interface in STM32F745IG

Hello Community!,I am working on STM32F745IG, where i am interfacing 24 SPI slaves to STM32F745IG MCU. Please let me know how many slaves can be connected to single SPI interface in STM32F745IG?. I looked into datasheet, I couldn't able to find. Than...

Resolved! STM32F4 using CCM data RAM for STACK and HEAP

Hi, I have STM32F407VET6 which has such memory layout.As I understand CCM data RAM is unused by default and just waits to be used? So can I move STACK and HEAP to it? How do I move it? (I did not find defined STACK address anywhere in KEIL project)Is...

0693W00000YA0E4QAL.png
JBond.1 by Senior II
  • 5375 Views
  • 3 replies
  • 2 kudos

NUCLEO-F767ZI mounting

Hi, We are developing a baseboard for the NUCLEO-F767ZI and use the ZIO connectors. Right beneath CN9, CN8, CN10 and CN7, there are mounting holes , that we want to use to make a robust mounting for industrial use. But the holes are very near and nor...

NUCLEO767-1.png
AAA by Associate
  • 1946 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.