STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H743BIT6

Hello,I'm using the STM32H743BIT6 microcontroller in a project, and I'm interested in utilizing USB_OTG for high-speed data transfer to  LabVIEW. I've come across some schematics that involve connecting USB_OTG pins to a USB Micro-AB connector. Howev...

image_2023_10_10T06_14_24_635Z.png

Resolved! H7 pin-to-pin compatability list ?

Hello,I was just shocked to see that H723 and H735 are NOT pin-to-pin compatible, at least in LQFP-144.Shoot, I thought I could switch between H723 / 725 / 733 / 735 if necessary. I found the list for F4 / F7 / H7 compatibility, is there another list...

LCE by Principal II
  • 5464 Views
  • 7 replies
  • 2 kudos

Resolved! Using Infineon HyperRAM with STM32L4R5

Hello,I am looking for advice in using an Infineon S27KS0642 64Mb HyperRAM chip on a STM32L4R5Z and configured via CUBE.I have it working, so I am pretty sure that the hardware is connected correctly and I can read and write successfully to it.  Howe...

AJJ by Associate II
  • 5495 Views
  • 9 replies
  • 1 kudos

Resolved! Circular DMA on ADC runs once and stops

I'm using an STM32H563. Setup to get ADC captures into a buffer using DMA in circular mode.I have TIM1 triggering an ADC1 conversion of two channels. And a buffer with 16 readings using DMA. The GPDMA is set in Standard Request Mode and Circular enab...

iguffick2 by Associate III
  • 3555 Views
  • 2 replies
  • 0 kudos

Resolved! STM32h725 Slave PSSI bad length

Hello,I'm trying to use the PSSI bus in slave mode to transmit data from a small FPGA. After some time chasing a weird bug (I'm losing 8 32bit words at the end of packet) I decided to use a logic analyzer on the bus and it showed a weird behavior fro...

mkhairy_0-1692434379099.png mkhairy_1-1692434419928.png USB_dump_start.png BUS_dump_start.png
mkhairy by Associate II
  • 11521 Views
  • 9 replies
  • 1 kudos

How to check CAN signal of CAN loopback mode in stm32f446RE

I have used an example code from STM of CAN loopback mode I have used a CAN transreceiver but i'm not getting how to check the signal as well as the data in CAN bus analyser please help me in hardware connection as well as how to check it in CAN bus ...

Komal by Associate III
  • 1073 Views
  • 0 replies
  • 0 kudos

how to print hello world in mcu boot using stm32f429zi board.

we r doing one task how to print hello world in mcu boot using stm 32 board . I KNOW THERE IS CONFIGURATION BUT NOT WORK properly we tried. there is one configuration CONFIG_BOOTLOADER_MCUBOOT=y which connect mcu boot code and application code. when...

VPati.2 by Associate II
  • 4204 Views
  • 7 replies
  • 0 kudos

Resolved! STM32F401 Datasheet Error? Vih

So table 54 Vih for 5V tolerant pins is 0.7Vdd. For Vdd 3.3V this is 2.31V.I'm having input capture trigger on signals that only reach 1.8V with 100% consistency on 4 pins.Most stm32f4 the Vih for the same pins is 0.45Vdd + 0.3V, which would be 1.65V...

TonyFauci by Associate II
  • 5193 Views
  • 9 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.