2023-10-11 4:16 AM
I am working with STM32U575, When building my project I am facing an issue.
The error is as follows:
C:/ST/STM32CubeIDE_1.13.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v8-m.main+fp/hard\libc_nano.a(libc_a-gettimeofdayr.o): in function `_gettimeofday_r':
Could somebody please help me how to resolve the issue.
Solved! Go to Solution.
2023-10-11 5:06 AM - edited 2023-10-11 5:39 AM
Hello @Mathil
maybe this post could help you :
https://community.st.com/t5/stm32cubeide-mcus/gettimeofday-r-error-come-while-i-am-building-with-latest-stm/td-p/579637
This issue will be fixed soon. At that time you have to define your own function. You can define it as "empty" and return 0, just to get rid of this warning message if you don't want to use it.
Else you can implement a function using the RTC to get the date and time after you have programming correctly the RTC calendar and time.
So you can add a file named time.c if not having one and then add the following empty function :
#include <sys/time.h>
int _gettimeofday( struct timeval *tv, void *tzvp )
{
// you can add code here.
return 0; // return non-zero for error
} // end _gettimeofday()
best regards
Mikael
2023-10-11 5:06 AM - edited 2023-10-11 5:39 AM
Hello @Mathil
maybe this post could help you :
https://community.st.com/t5/stm32cubeide-mcus/gettimeofday-r-error-come-while-i-am-building-with-latest-stm/td-p/579637
This issue will be fixed soon. At that time you have to define your own function. You can define it as "empty" and return 0, just to get rid of this warning message if you don't want to use it.
Else you can implement a function using the RTC to get the date and time after you have programming correctly the RTC calendar and time.
So you can add a file named time.c if not having one and then add the following empty function :
#include <sys/time.h>
int _gettimeofday( struct timeval *tv, void *tzvp )
{
// you can add code here.
return 0; // return non-zero for error
} // end _gettimeofday()
best regards
Mikael
2023-10-12 2:28 AM
@MikaelM Thank you for the solution.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.