STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interrupt on in B1? ON Bluepill STM32F103 without HAL

Hallo,does anybody have an Example(without HAL), how I can initialize an external Interrupt with STM32F103 Bluepill on PIN B1?At this moment I try with this[code]procedure Event(); iv IVT_INT_EXTI1; ics ICS_AUTO;beginGPIOC_ODR := not GPIOC_ODR; // To...

sven by Associate II
  • 1006 Views
  • 0 replies
  • 0 kudos

STM32F407VG ADC DMA Interleaved Mode

Good morning to everyone,I am trying to obtain on STM32F407VG Discovery a sampling of a signal with interleaved mode. I am experiencing problems, mainly I see that it does not enter the routine commanded by the adc flag. Would anyone be able to help ...

davidec by Associate III
  • 3174 Views
  • 4 replies
  • 1 kudos

Resolved! Rising and falling edge on GPIO_STM32G4

Hi,I am working with STM32G491RE.I am giving pulse to GPIO pin from function generator. That pulse will be 2 msec on time and 8msec off time.I need to make flag high if the signal from function generator lost.Can anyone suggest me how to do this?void...

sireevenkat1_0-1696936253459.jpeg

Resolved! STM32L0x2 timer frequency off by 10%

Hello!I'm trying to setup up timer6, i need to use it at different frequencies at different times. To test the timer i toggle an output pin in the ISR and measure the frequency with an oscilloscope, but the frequency is consistently off by about 10%....

Fiskk by Associate
  • 2526 Views
  • 3 replies
  • 3 kudos

Resolved! Compatibility of different footprints of same MCU type

Hello,I want to change the MCU STM32F779AIY to STM32F779NIH6I already checked the pinout in CubeMX and i can use the same config for the peripherals at the same naming of pins (PB1, PA4 and so on).Do i need to change anything at the software if i cha...

Resolved! stm32f429-Disc1

What is the minimum and maximum voltage the internal ADC of stm32f429 can measure ?

harry123 by Senior II
  • 4219 Views
  • 7 replies
  • 2 kudos

STM fgets character limit

fgets ignores my limit and is trying to read 1024 characters.char *fgets( char *str, int numChars, FILE *stream );as I understand fgets it is supposed to read up to numCHars characters from stream into str. It should also stop on a newlineThe behavio...

Qye by Associate II
  • 2362 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.