Resolved! Process Technology of STM32L4R9I-EVAL evaluation board
Dear admin,I would like to know which process technology (?nm) of STM32L4R9I-EVAL evaluation board.I've checked the user manual but not having this information. Thanks & Best Regards
Ask questions, find answers, and share insights on STM32 products and their technical features.
Dear admin,I would like to know which process technology (?nm) of STM32L4R9I-EVAL evaluation board.I've checked the user manual but not having this information. Thanks & Best Regards
Do you think is possible add a second lcd display to this evaluation board also without touch screen ?
stm32 family atleast 1 CAN Interface on it. if any suggestion please revert me.
Hi, I want to use UART with DMA on my STM32F407 MCU. I would expect that it would trigger `HAL_UART_TxCpltCallback` interrupt on transfer complete, but it does not do that. I tried many different configurations in STM32CubeMX:enabling "USART2 global ...
Hello,I am trying to use the DFSDM module on the Nucleo-H743ZI2 board .As a minimal example, i tried to use a sinc filter of 2. order with a FOSR of 4.Channel0 is activated in the parallel mode, standard data packing mode and the setting to take data...
I use STM32L496To save current to a minimum, It briefly enters NOMAL mode (0.2mA ~ 6.3mA) and updates the LCD numbers, then stays in STOP mode (0.2mA) for about 1 second and then wakes up with RTC.I keep repeating this.However, in STOP mode, it alway...
Hi! Noticed a typo in the system configuration controller (SYSCFG) register map in both reference manuals RM0399 (Rev 4) and RM0433 (Rev 8). The SYSCFG_CCCR register is at two different offsets (0x28 and 0x2C) and SYSCFG_PWRCR is missing. I think, S...
Hi i have a generic doubt about falsh wait states:Say we configured the PLL to run system core clock at 160 M Hz, with flash wait states as 5.Then is cpu is equvilent to 32 MHZ core performance? (assuming 1 clk/ 1 inst, no ART's)Could some one help m...
I want to interface N25Q.. External NOR flash with STM32F469. Where I want to load and execute the code from N25Q External flash memory using QSPI memory mapped mode.Is this solution is Possible?If yes, from where I can get support?
Hello,I have a strange issue here trying to read 2x PDM mics from the SAI peripheral and output the audio over the I2S peripheral here on the H7.I use what appears to be the correct frequency for both peripherals and clear audio coming out, until the...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.