STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! B-U585I-IOT02A Dev Kit: WiFi and Bluetooth Module Part Numbers?

Looking for Part numbers for modules on the B-U585I-IOT02A dev kit, specifically the Bluetooth and WiFi modules, but also looking for part numbers on the modules listed below. Didn't see P/N's listed in the datasheet but maybe I was looking in the wr...

PNada.3 by Associate II
  • 2026 Views
  • 2 replies
  • 1 kudos

Resolved! Bring up stm32G4 custom board

Hi,In my project I need to bring up stm32g4 IC in custom board. Can anyone tell me the process to do that.1. Bootlooader flashing: Do we need to flash the bootloade in to IC?if Yes,Where can I get the bootloader for STM32G4 IC.What is the process to ...

Resolved! Evaluation Kit for STM32H745XI

Hi,We are using STM32H745XI processor for one of our customer products. To start our initial software prototype development, we are looking for the evaluation kit. I went through the processor product page, and I have following queries:1. Looks like ...

Jigs by Associate
  • 1446 Views
  • 1 replies
  • 0 kudos

STM32F746 FMC NWE periodically goes high

Hello. I'm using STM32F745VET.I want to connect SRAM via FMC, but when I run a simple app, the waveform look like below.The code I made is just write data "0x28". and It does not work.As you see, NWE signal work high-low periodically. I think this is...

image.png
Kourinho by Associate
  • 1981 Views
  • 3 replies
  • 0 kudos

TIMER

Hello,I found an example on the internet of a project but I don't understand the usefulness of using a Timer 7. Could you tell me why ? Thanks in advance. __IO uint32_t usTick; void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) { /* Preven...

DYann.1 by Senior II
  • 15477 Views
  • 40 replies
  • 3 kudos

Strange behavour when coming out of standby mode

Hi  I have my own board with a STM32L433 , running on a battery. I place the processor in Standby mode, then exit it with the RTC AlarmA and periodic timer. As soon as it wakes up I initialize the uart and display a message on the terminal .When put ...

Noise/Feedback on STM32H735G-DK when using line-in audio

I'm trying to prototype an audio effects unit with the STM32H735G-DK board. I am using the line-in input jack and output (headphone/line-out) jack. There was no example using the line-in jack for the 35G-DK board as far as I could find. So I just ref...

nick9871 by Associate II
  • 5066 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.