STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Jump to Bootloader to UART Programming - Timeout error

Hi, I need to create a system for which it is possible to update the firmware remotely.My system communicates with a serial port (RS422) with a PC, and through this serial I would also like to update the firmware. Obviously without moving the BOOT0 p...

FMass.1 by Associate III
  • 3062 Views
  • 2 replies
  • 0 kudos

Resolved! STM3210E-EVAL won't receive UART

Hello, I'm building a communication between two devices an Arduino Mega 2560 and STM3210E-EVAL. For the communication I need to use RS232. In between the two devices I use the MAX232. I got it working one way where the STM32 sends 1 byte to the Ardui...

Smdeint by Associate III
  • 3177 Views
  • 2 replies
  • 0 kudos

I almost dont want to ask the question...

Hello.I may be on a fools errand here. I have a STM32U5A9J-DK kit obtained by work, for work. I work for a medical devices company and I get to decide what hardware is used in one of our main medical telestration products. I have endless hardware exp...

Z8000 by Associate
  • 6155 Views
  • 9 replies
  • 5 kudos

flash related issues of STM32F103 series

When using the STM32F103 series, it is occasionally found that the content of some flash addresses will be automatically written as 0xFF when powering on.and sometimes it's written as 0x00.I want to know why does this happen? or under what circumstan...

liuxc by Associate
  • 1785 Views
  • 1 replies
  • 0 kudos

STM32L4A6 GPIO PC8 pin can't be pulled to low

Hi,i Pin PC8 is configured as GPIO,  but unfortuately, after execute following codesHAL_GPIO_WritePin(GPIOC, GPIO_PIN_8, GPIO_PIN_SET) andHAL_GPIO_WritePin(GPIOC, GPIO_PIN_8, GPIO_PIN_RESET) , the pin status didn't change, always keeps in High status...

Owenlu by Associate II
  • 2421 Views
  • 4 replies
  • 0 kudos

Resolved! Questions regarding ADC ON STM32

Hi All,I'm starting to get familiar with the STM32 Series of Microprocessors and I'm completing some exercises using a mixture of direct writting to peripherals and low level ST libraries using the CUBEMX to get familiar with the chips. I'm using the...

cdtsilva by Associate
  • 3631 Views
  • 3 replies
  • 1 kudos

STM32G474 error code

Hi, I'm using STM32G474RET6 for development.When I debug code by SWD, the download verified successfully.But it will be suspended at HAL_Init() and show an error is Break at address "0x1fff5048" with no debug information available, or outside of prog...

Stone1_0-1698818507459.png Stone1_1-1698818516062.png
Stone1 by Associate II
  • 4404 Views
  • 8 replies
  • 0 kudos

Beginner`s ask for help to flash the STM32

Hi,I am an absolute beginner in STM32 ecosystem. This is my first time programing an STM32. My MCU is STM32F756VGH6 in TFBGA100 package. I wrote a simple led blink program and encountered a problem while trying to flash the MCU (got some kind of erro...

Vilius by Associate III
  • 49172 Views
  • 41 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.