STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI documentation mismatch with CubeMX

Posted on March 26, 2017 at 23:53I'm using CubeMX 4.19.0 for STM32F407G-DISC1 and firmware for STM32F4 version 1.14.0. (yes I realize there is an update).When setting up an SPI port, one of the parameters is CPHA, the clock phasing. You have to decl...

G431KB abnormal current consumption

Suddenly the CPU has started to absorb 160 mA. At the beginning, when I started using it, it was 30 mA. I cannot understand the reason. No hardware modification has been operated. Has anybody experienced anything like this? Thanks in advance.@apoggia...

gigikw by Associate
  • 1073 Views
  • 1 replies
  • 0 kudos

STM32L471RGT6 32 bit SPI

Hi is it possible to communicate 32 bit data over the SPI bus? Using IOC to set up the SPI port 2 , I seem to be limited to 16 bits.Thanks a lot  Richard  

rwils.1 by Associate III
  • 2407 Views
  • 5 replies
  • 0 kudos

STM32F0 Discovery board

Hi,   I am new to work on STM32F0RB discovery board to get update the FW through UART/USB port. If any one have the idea to work on this please give me the solution.   Thanks, Shashi Shekhar

Resolved! STM32H723VG using Timer outputs as GPIO Output

Hi community!I have a STM32H723VG and I use Timer1 on that device to generate complementary PWM Outputs (Chx + ChxN) on channel 1-3 plus a 1-channel PWM on Channel 4. When the PWM is not needed, I have to set the output pins of the timer either high ...

CBerg by Senior II
  • 3082 Views
  • 1 replies
  • 0 kudos

STM32C011 System/Open Bootloader

Hello,I'm using an STM32C011 for a product we are developing, and I want to use ST's default System/OpenBootloader (via UART) that the virgin chips have on board. That way in production we don't have to download our custom bootloader, and we'll use t...

starivore by Associate II
  • 7113 Views
  • 8 replies
  • 5 kudos

32H563Zi can't work in VDD=1.8V?

Hi, Sir: Currently using H563ZI (MB1404C) to develop programs.When VDD=3.3V, MCU works normallyWhen VDD=1.8V, the MCU functions abnormally (USB function fail), but the specification indicates that it can support VDD=1.8V. Where should I set this on t...

Charles63 by Associate II
  • 1990 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.