cancel
Showing results for 
Search instead for 
Did you mean: 

Nonsense in STM32L452E Reference Manual, RM0394 Rev 4 - 2018!!

https://www.st.com/resource/en/reference_manual/rm0394-stm32l41xxx42xxx43xxx44xxx45xxx46xxx-advanced-armbased-32bit-mcus-stmicroelectronics.pdf

Cross-references the wrong register, should be RCC_BDCR

RM0394 Reset and clock control (RCC)  Pg 247
6.2.6 LSE clock

...

External source (LSE bypass)
In this mode, an external clock source must be provided. It can have a frequency of up to 1 MHz. You select this mode by setting the LSEBYP and LSEON bits in the AHB1 peripheral clocks enable in Sleep and Stop modes register (RCC_AHB1SMENR). The external clock signal (square, sinus or triangle) with ~50 % duty cycle has to drive the OSC32_IN pin while the OSC32_OUT pin can be used as GPIO. See Figure 14.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
STTwo-32
ST Employee

Hello @Tesla DeLorean,

Thank you for reporting this. I will check it internally and get back to you as soon as possible.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

STTwo-32
ST Employee

Hi @Tesla DeLorean 

I've escalated this to the appropriate team for correction of RM0394 with internal ticket ID165919.

(PS: ID165919 is an internal tracking number and is not accessible or usable by customers)

thank you for your contribution.

Best Regards.

STTwo-32.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.