STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

multichannel adc

why i am getting same values in all channels please someone helpvoid Adc_Vbat(void) { ADC_ChannelConfTypeDef sConfig = {0}; sConfig.Channel = ADC_CHANNEL_16; sConfig.Rank = 1; sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_1; if (HAL_ADC_...

meena by Associate III
  • 1433 Views
  • 3 replies
  • 0 kudos

M7 with 4xRAM ICs over FMC

Hi,We have a question about a system design we would like to implement for our product.We are working with the STMF32F723 MCU and are developing our own HW. We need 216MByte of RAM for our application and would like to implement it with the functiona...

CObri1_1-1695644204144.png CObri1_1-1695643333384.png
CObri.1 by Associate III
  • 5419 Views
  • 10 replies
  • 1 kudos

STM32L452 Temperature

Hi,How can we extract a correct reading of the internal temperature of the STM32L452 in degree C?We currently read a number '141' but this is clearly not the CPU temperature which should be 22-28oCWe have followed the general app note on temperature ...

H7 single-core vs. dual-core

Hi,I am considering which solution to go for in a new product. To start with, I am going for a 480 MHz STM32H7 with high-resolution timer (HRTIM) for some quick PWM regulation. The regulation feedback is supposed to come from a fast ADC, so I need to...

EThom.3 by Senior III
  • 8241 Views
  • 10 replies
  • 3 kudos

Resolved! CAN FD multiple MCUs

I am trying to connect 2 NUCLEO-G0B1RET6 boards,using CAN FD. I previously did it using CAN, But now i am trying to connect these boards using CAN FD. So far no success,I want to know if it is possible to do it using CANFD.Kindly help me in this rega...

Resolved! USB host on STM32L475 board with FATFS

Hi! Hope everyone are doing well! I currently encounter a problem and can't solve it. I want to write some pieces of data into a file in a usb-disk and now the Appli_state is constantly idle even I connect the USB-Disk already.This is a test demo cod...

ZZY_0-1700078072221.png ZZY_0-1700078428443.png
ZZY by Associate II
  • 3279 Views
  • 5 replies
  • 0 kudos

Resolved! STM32L4 - Could state of JTDI pin affect switch-over to SWD?

I am using a STM32L471 MCU in a design that may be flashed with new firmware in situ. I'm using SWD as the interface, so the two unneeded JTAG pins (JTDI and JTDO) are used for other purposes. According to the reference manual, JTAG is activated by d...

oscarw by Associate II
  • 4526 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.