STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI DMA transfer issue on STM32H743

 I am reaching out to seek your expertise regarding the DMA transfer issue on SPI that I encountered while using the STM32H743 microcontroller.When an EXTI LINE 0 event (data ready) occurs, attached to the code is a program in which 30 bytes of 0xFF ...

oseaw.1 by Associate II
  • 6402 Views
  • 5 replies
  • 0 kudos

Resolved! How to send an image located on a USB drive to the display?

ILI9341 display  connected to STM32F407VGT6The USB drive is connected to the STM32F407VGT6, this USB drive contains images, I need to send these images to the display. I already know how to send to the display an array that is located on a USB drive....

MMust.5 by Senior II
  • 4600 Views
  • 8 replies
  • 2 kudos

STM32F407 I2C INA232 Problem

Hi everyone,I am using STM32F407 to read voltage and current values from INA232 and TCA9548.I have 8 INA232 so I used TCA9548 as I2C Switch.I have coded as follows:1. SET TCA9548 on Port 12. Read the voltage value on INA232 at port 1The result I get ...

Hoi_0-1700039106263.png Hoi_0-1700042387194.png Hoi_1-1700042577069.png
Hoi by Associate II
  • 2337 Views
  • 1 replies
  • 0 kudos

ADC calibration issue

Hi , I am trying to calibrate ADC in STM32334R8. But the code is stoping at calibration phase itself. I will attach the initilization code below for your reference.  LL_ADC_Disable(ADC1);LL_GPIO_ResetOutputPin(GPIOC,LL_GPIO_PIN_8);LL_ADC_EnableIntern...

vasudev by Associate II
  • 1853 Views
  • 1 replies
  • 0 kudos

Upload .bin files on windowsthrough the USB interface

Hi, I just decided to try mbed OS 6 for programming my NUCLEO-WB15CC. Compilation is successful, but when i try to flash the compiled .bin file, the operation fails saying that a device was not connected even though it was. I am guessing it is becaus...

Elijah1 by Associate
  • 1972 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F44 MCU: Read protection flag not removed

HiI try to implement the read protection on my STM32F44 board based on this example:https://community.st.com/t5/stm32-mcus/how-to-change-the-read-out-protection-on-stm32f4/ta-p/49410In principle, it works, but I have some strange behavior. My code:if...

Corono by Associate III
  • 5751 Views
  • 5 replies
  • 0 kudos

Conditional data watchpoint with debugger or DWT

I've tried both Eclipse and the VSCode Cortex debug plugin to set a conditional watchpoint but both fail (break every access irrespective of value). This I guess is due to OpenOCD not supporting the multiple compare registers in the DWT that are requ...

Resolved! HRTIM,ADC

I am using hrtim to trigger the adc, but if the regular channel is not triggered with hrtim, it doesn't go into the interrupt of the ADC properly, I checked a lot of information and didn't find a solution, here is my code and cubemx configuration: N...

iskan_0-1695092649603.png iskan_1-1695092655031.png iskan_2-1695092661369.png
iskan by Associate III
  • 2749 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.