STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How the stack work?

Hi there,I remember the stack starts from the top, which means the earlier local variable will be located at a higher address space. I have the following code in the main() function in ARM-MDK IDE:  uint8_t v1; uint8_t v2; uint8_t v3; LOG_DBG("&v1[%p...

Junde by Senior III
  • 4495 Views
  • 6 replies
  • 2 kudos

STLINK-V3SET allows programming but not debugging

I've an STLINK-V3SET and while trying to connect with my board, it does detect the chip but I'm unable to debug. Works fine with stm32 programmer but I'm unable to debug program on stm32 cube ide.Connections:STLINK -- BoardGND --> GNDDIO  --> SWDIOCL...

Ans by Associate III
  • 1400 Views
  • 1 replies
  • 0 kudos

Resolved! Processor crash on PG10 initialisation

Hi all,I am in the process of bringing up a prototype board with a STM32L4R7ZIT6. I'm using CubeMX and use it for generating the startup code. I've configured a lot of peripherals.When I configure PG10 as an input, the CPU crashes. Exactly at the mom...

GeertZelf by Associate III
  • 10346 Views
  • 17 replies
  • 3 kudos

Can't able to upload code in STM nucleo-u575zu-q

we are using STM nucleo-u575zi-q module, when I try to connect with pc its indicating the error with this failed txt file, need help to rectify this issue, Due to this issue we are unable to upload new code to this controller, please help us to resol...

Raja2 by Associate
  • 1850 Views
  • 1 replies
  • 0 kudos

Resolved! Best practices for instrumentation logging with dual-core MCU

Hi all,  May I kindly ask some suggestions about the best practices, how to use e.g. printf for instrumenting logs that both of the dual M7 and M4 core could print at the same time?(Best case is through the same port...)  Some background information:...

Leon_MS by Associate III
  • 5045 Views
  • 8 replies
  • 1 kudos

STM32F7 QSPI Fast Read Quad Problems

I am here again to ask for your help :)I am using a STM32F767ZI Nucleo Board and connected a Winbond W25Q64JV using the QSPI interface of the MCU. Everything is working fine so far - I can read data in every mode described in the data sheet (even Fas...

_legacyfs_online_stmicro_images_0693W00000bjUJuQAM.png
PUrsu.1 by Associate II
  • 9976 Views
  • 12 replies
  • 0 kudos

Resolved! LPTIM stops working when RTC is activated

Hello,I started with configuring all 4 of the U5's LPTIMs to "Count internal clock events", sourcing all of them with LSE and using different period values for each. The autogenerated code (STM32CubeIDE v1.13.2) worked, meaning each timer toggled ind...

EC.3 by Associate III
  • 2950 Views
  • 2 replies
  • 1 kudos

Special I2C slave , how solve wakeing masters

My problem is i require emulate with STM I2C chip , that requires wake adr send before comm. But normal slave code isnt handle this.Signals on bus (FYI master is other device no STM)as can see master send one adr without data and repeat, first reply ...

MM1_0-1700064978907.png
MM..1 by Chief III
  • 2546 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.