STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U5 Can't exit STOP2 mode with LPTIM

Hi everyone,I'm trying to enter STOP2 mode with a STM32U575 and exit from it with a LPTIM1 compare match. LPTIM1 is clocked with LSE, so it should be still working in STOP2 mode.Here is part of my code in the main funtion: /* Initialize all configure...

LMenc.1 by Associate II
  • 4943 Views
  • 5 replies
  • 0 kudos

STM32H723 ULPI compatible devices

Hi All.This is my first post here.I am in process of developing a device with STM32H723(100pin) which must have USB HS device functionality.I found a number of different HS ULPI PHY chips like USB330, USB3320C, FUSB2805MLX etc.During searching info a...

MikeEmbedded_0-1698785934823.png

static memory zeroed at system reset

At system reset, static memory is zeroed.  I want static memory to be entirely left alone by the system.  I want the memory to have what I put in it, not clobbered.  Granted, I have to retain power to the device, but static memory should be able to r...

Resolved! Can FDCAN work with CAN 2.0B devices?

I am working on a project where the requirement for the microcontroller is to communicate over the CAN bus. The STM32G0B1KET6 is having FDCAN controller inside. It mentions in the datasheet that "The CAN modules are compliant with ISO 11898-1 (CAN pr...

anuj by Associate II
  • 15279 Views
  • 7 replies
  • 0 kudos

LUT Configuration

Hi,I need help about LUT configuration of a custom display. I am using STM32L4R9-Disco board. The LUT for the display is given in .xlsx format. However, I am using another display of size 454x454 with that board. Is there any way to generate LUT for ...

SSG by Associate II
  • 3965 Views
  • 4 replies
  • 0 kudos

Resolved! LSERDY is set, but LSE not running correctly

Hi, I am working on a project for STM32F746ZGT6 that uses the RTC clocked from the LSE.In some cases I am seeing an issue where the LSE appears to start (LSERDY reads as 1 within the call to HAL_RCC_OscConfig from the peripheral libraries) but it app...

AMill.7 by Associate
  • 2800 Views
  • 3 replies
  • 0 kudos

XNUCLEOBNRG2A1 and NUCLEOU575

Hi,I picked up a X-NUCLEO-BNRG2A1, and I am trying to communicate with it through a Nucleo-U575 Board. I basically generated a project template through CubeMX for the STM32U575 and included the BlueNRG-2 (X-CUBE-BLE2) Pack to include Bluetooth HCL/AC...

IVent.1 by Senior
  • 4569 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.