STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Difficulty with speed of updating PWM duty cycle

Hi, I'm a relatively new programmer, attempting to program a "Bluepill" module, which has the STM32F103C8T6 microcontroller. I'd like to be able to quickly change the duty cycle on a PWM output, so that I can adjust the position of a servo motor as I...

Bought a STM32 NUCLEO-F411RE and "No ST-Link Device Connected"

Hi All, i'm quite new to the world of embedded and only recently moved off MCU's like the ESP32.I just bought a STM32 Nucleo board and when I went to use it with the cubeIDE I got the error "No ST-Link Device Connected". I installed the drivers STSW-...

Kesan by Associate II
  • 4473 Views
  • 8 replies
  • 1 kudos

Resolved! KEIL uVision5 is closed suddenly

I have Nucelo-F492 and I used STM32Cube on 2022 successfully without any problem. This was very easy. I am attending now a training course in "RTOS by using Keil uVision", But every time I use Keil to erase or download programs in my Nucleo, Keil uVi...

Hasan by Associate II
  • 4632 Views
  • 2 replies
  • 2 kudos

Resolved! Building Example for Nucleo-429ZI

Hi, I am new in STM32 MCU. I have bought Nucleo F429ZI, I downloaded and installed STM32CubeIDE. I have selected a new project, then I selected some examples for Nucleo-F429ZI. The name of the project is GPIO-IOToggle. I made a build without making a...

Hasan_0-1700328837325.png
Hasan by Associate II
  • 2466 Views
  • 2 replies
  • 0 kudos

Help with i2c slave device

Hi, I want to implement an I2C slave with a STM32L476 micro that basically behaves like a memory. Therefore it must respond to another micro which executes the HAL_I2C_Mem_Write() and HAL_I2C_Mem_Read() operations to this slave.Searching on the inter...

FMass.1 by Associate III
  • 3924 Views
  • 6 replies
  • 0 kudos

STM32F103 ADC+DMA+USB -> what is a reasonable speed?

Posted on May 11, 2018 at 00:41I am trying to use a STM32F103 as a sampling device to sample a signal at a rate of 200-300kHz for multiple seconds. Using CubeMX the ADC conversion was configured and DMA using a circular buffer was applied. This all ...

STM32: To achieve high speed over usb2.0 @60Mhz

Hello Team,I have developed a custom board having external PHY to drive USB in HS mode. The board consist of STM32h743zit6 controller and PHY from microchip USB3320C driven by an external clock of 52 Mhz.Although the configuration has setup using CDC...

Resolved! RTC not rolling over at midnight

Using the RTC on a NUCLEO-G071RB (HAL) I have a program the prints out the time, date and temperature in degrees Centigrade. I left it running overnight and discovered in the morning that the hours had not reset to 00:00 at midnight and neither had t...

Dabbo by Associate III
  • 3318 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.