STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DMA is not working on STM32H747i-DISCO board

I am working with STM32H747i-DISCO  board and I configured ADC1 with DMA1 stream0 and ADC3 with DMA2 stream0 both with Cortex-M7 core as initializer and I created the MDK-ARM project using STM32Cubemx and compile the code in CrossWorks when I debug t...

Resolved! Revision code

Hi To what does the revision code correspond?I have not found any clear answer in the documentation.Does a new revision replace the previous one? if so how to know which one is the most recent.

Saredo by Associate III
  • 1736 Views
  • 1 replies
  • 1 kudos

Getting HAL_ERROR while using I2C in Fast mode pulse

Hi All,I trying to interface MAX6651 Device using I2C module using STM32F410C8U6 MCU.Device address is 0x36 But when i'm using HAL_FMPI2C_IsDeviceReady(&hfmpi2c1, 0x36 , 2, 100); this API returning the valueHAL_ERROR.Here are some snaps Anybody look ...

Screenshot 2023-11-07 151633.png Screenshot 2023-11-07 151523.png

STM32 HRTIM BURST DMA CONFIGURATION

Hi all,I am trying to configure burst dma on my board (stm32g474). I have successfully configure the dma for single register, however, when I want to configure dma for more than one register, I failed to do that as it only allow me to fill one addres...

OFN by Associate II
  • 2637 Views
  • 2 replies
  • 0 kudos

STM32G0B1 Options Bytes

Dear, I currently use a STM32G0B1 on a custom board ans all worked fine until now. My firmware change the options bytes at running to disable the dual bank and using and single bank Flash.At the power up, the firmware check the options bytes and chan...

YDann.7 by Associate III
  • 10552 Views
  • 8 replies
  • 0 kudos

Resolved! Problem with I2C Interface on STM32F469I-DISCO

Hello, I am trying to write something on the I2C bus to a digital potineometer using the STM32F469I-DISCO board but I get no result, even no response from the device and its like there is no device connected on the bus. I tried the same potineometer ...

mids400 by Associate III
  • 3017 Views
  • 3 replies
  • 1 kudos

Resolved! How to switch a pin between open drain and ground

Hi, I have a pin labeled "DISABLE_HV" that I want switch between open drain and ground (and vice versa) to switch-off and switch-on a DC-DC converter. How can I implement this functionality in the code using HAL library?

ECiot.1 by Associate II
  • 6364 Views
  • 4 replies
  • 1 kudos

Resolved! LPTimer counts only to 1 if running on LSE

Hi, I'm using on a STM32L4R9 a LPTimer1 in interrupt mode. If i use it with the PCLK1, HSI or LSI as clocksource it works as expected. It counts to the ARR value and then the interrupt occours. If i use the LSE as clocksource the LPTimer seems only t...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.