STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART in Interrupt mode Stuck??

Hello all,I'm using STM32 F103CBT6 MCU on a custom board where MAXRS485 is used. Rx and Tx of the Modbus chip is connected to USART1 on the MCU.To receive and Transmit data I'm using UART in interrupt mode. The program also has 8 GPIO interrupts on m...

GSaw by Associate II
  • 5942 Views
  • 3 replies
  • 0 kudos

Resolved! ADC Conversion time and Sampling time

I have an stm32f407g.In the reference manual (in the ADC section) I found several terms I am afraid I have confused between them.I would like to explain my reasoning with an example and get your feedback if I said something wrong. -------------------...

SmartSelect_20231116_182919_Samsung Notes_1 (1).png luke514_1-1700220904367.png luke514_0-1700220452982.png
luke514 by Senior
  • 32364 Views
  • 7 replies
  • 4 kudos

Resolved! VREFBUF not working on STM32WLE5JC

Hello everyone,I'm trying to set up VREFBUF as an internal reference at 2.5V, but the configuration isn't working. I've seen there were issues with this (VREFBUF Enable Problem - STMicroelectronics Community), but even after rearranging the function ...

grf14 by Associate
  • 1418 Views
  • 1 replies
  • 0 kudos

Resolved! ADC signal noise

Hi, I'm using stm32f429 disc1 adc1 PA4 and GND to get the ADC signal, the voltage of the signal is 300 mV. The signal that I'm getting after conversion has some noise, But the same signal when seen through an oscilloscope has no noise. The noise or d...

harry123 by Senior II
  • 2212 Views
  • 2 replies
  • 3 kudos

I2C error in sending data (for the oscilloscope)

Hello ! I've got a problem because I tried to check the SDA and SCL pins like in the picture :  Sorry for the paint picture (the oscilloscope was during classes so I don't have it right now).The output was all the time noises even thought the code wa...

Xenon02_0-1700670192061.png Xenon02_1-1700670341278.png Xenon02_2-1700670423029.png Xenon02_3-1700670458974.png
Xenon02 by Senior
  • 6387 Views
  • 10 replies
  • 0 kudos

simple LWIP UDP project not working with latest Cubmx 9.6.2

Hi,I'm using STM32H743ZI with STM32CubeMX 6.9.2 and STM32CubeIDE 1.13.1.I added new STM32 project using the CubeIDE GUI - selected the STM32H743ZI device and automatically the project was generated, I opend the IOC file and enabled the ETH + LWIP opt...

Mz1_0-1700046225542.png
Mz.1 by Associate III
  • 6467 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.