2023-11-22 5:45 AM - last edited on 2023-11-22 7:27 AM by Mike_ST
I am working with STM32H747i-DISCO board and I configured ADC1 with DMA1 stream0 and ADC3 with DMA2 stream0 both with Cortex-M7 core as initializer and I created the MDK-ARM project using STM32Cubemx and compile the code in CrossWorks when I debug the M7 core DMA will not work and I checked with debug point inside the callback cursor will not enter into the callback function. But the same configuration I did in STM32CubeID and debug both the cores it is working fine but when I debug only M7 core it is not working with DMA.
2023-11-22 6:29 AM
Might need to post more info than just "it isn't working". Not mind readers here.
2023-11-22 10:07 AM
Hello @Pavankumar1,
May be this article can help you, as explains the issue with the DMA in STM32H7
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.