STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Saving Preset Data to STM32F373

I have an app running on an STM32F373 and need to save 'presets' as persistent non-volatile data.  Each preset is 500bytes and I would like to save at least 100 presets.What is the simplest method?  Should I use a removable SD card type solution, or ...

LMorr.3 by Senior II
  • 1461 Views
  • 1 replies
  • 1 kudos

How to configure the SAI with a CODEC

Hello, I would like to know if there are people who have already configured the SAI with a CODEC to recover the data ? With this link below: https://wiki.st.com/stm32mpu/wiki/SAI_device_tree_configuration I can see this figure but I don't quite under...

DYann1_0-1700559816623.png
DYann.1 by Senior II
  • 8359 Views
  • 8 replies
  • 0 kudos

stm32f767zgt6 usart1 and spi4 not working

I have issues getting usart1 and spi4 to work..USART1 "supposedly" work (software side do not complain) but USART1_TX pin is dead, there is nothing exiting this pin, scope shows it is dead. Same on multiple stm32f767zgt6 chips so it is not a dead chi...

arhi by Associate III
  • 3473 Views
  • 9 replies
  • 0 kudos

SRAM turn around delay

hi,i am using STM32H743BIT6 and SRAM IS62WV51216EBLL-55TLI.i want to calculate the SRAM turn around delay or TAT (Turn Around Time)?

Resolved! Failed attempt on using 2 Timers to Toggle GPIO.

Hello , I have initialized two timers , Timer3 and Timer9. Im using Timer9 with 137uS period , setting my gpio pin high , starting Tim3 Interrupt with 54uS period for now .When Tim3 Interrupt occurs I simply reset my gpio pin.My problem is that I sho...

PWM Actual.jpeg PWM_Orginal.png
Oahme.1 by Associate III
  • 8456 Views
  • 14 replies
  • 5 kudos

Jitter between ADC1 and ADC2 in ADC + DMA

First of all: I am aware ofhttps://community.st.com/t5/stm32-mcus-products/jitter-in-adc-dma-mode/m-p/231446#M51827but cannot see how the accepted answer solves the (my?) issue.Setup description:I useSTM32H723VGHxADC1 and ADC2 are setup inDual regula...

AndreasInhofer_0-1700646619735.png AndreasInhofer_1-1700646635388.png bad.png better.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.