STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Please use B&W text in documentation

In some newer STM32 documents, such as ES0418, text is rendered in various tints of blue. This results in decreased readability and problems when printing.Can ST please constrain fancy color schemes to marketing material, and use conservative black-o...

Resolved! Advice, please, how to view the function call tree and the contents of the MCU stack using STM32Cubeide. After the program crashes in debug the program loops in Hard_Fault_Handler () and it is not clear what cause such event.

What ability to view the contents of the call stack in CubeIDE is present?, i.e. what functions were called before the crash, preferably in the form of a tree

olezhandr by Associate III
  • 13534 Views
  • 9 replies
  • 7 kudos

Resolved! STM32L5 System View Description

The system view description files for H5 and U5 are on the website, but it is not for L5 (https://www.st.com/en/microcontrollers-microprocessors/stm32l5-series.html#cad-resources). Where can I find it ?

mete by Senior II
  • 2345 Views
  • 4 replies
  • 0 kudos

PWM generation TIM1 CH1N

I am trying to generate a regular PWM signal using TIM1 CH1N on the STM32-F411RE (pin PA7). I've seen a few posts on generating PWM using the advanced timers but nothing has seemed to work. The code below is the automatically generated code called in...

ctd962 by Associate
  • 12732 Views
  • 4 replies
  • 4 kudos

STM32F405 GPIO pin

As shown above picture, I got my STM32F405 configured as open drain to drive the led that is connected.Also, the same pin connected to via hex inverted (74HCS04D) to invert it and connected to OR gate. But when the GPIO pin in reset (low) state volta...

STM32.jpg
cjaya.2 by Associate II
  • 2439 Views
  • 3 replies
  • 2 kudos

Resolved! Timer synchronization

Hello Everyone i am using stm32G031J6 Microcontroller. I want to generate a PWM signal from Timer 1 working as slave in gated mode, that has a pulse width = 10us and pulse period = 44us  In this microcontroller i am using Timer 3 as a Master which ha...

PAN12 by Associate II
  • 12407 Views
  • 11 replies
  • 1 kudos

Ping not work on STM32L475 ETH

Hi, I'm trying to get the ethernet interface to work on an STM32H745. After fixing various hardware problems, now I don't just have software problems.I created a simple project with CubeMX, basically I did these things:- Enabled ethrmnet interfaces- ...

FMass1_1-1701356086728.png
FMass.1 by Associate III
  • 5255 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.