STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Good options to store public key in stm32h753

Hi, I am using a stm32h753 controller for my project, in which I need to store public key which could be updated during runtime. Is there any way I could store it inside the controller securely? Also do the stm32h753's flash has OTP? I could not find...

aswath by Associate II
  • 3539 Views
  • 4 replies
  • 1 kudos

NUCLEO-H723ZG ADC with DMA

HeyI am working with NUCLEO-H723ZG. I try to sample signal of sine wave at 25KHz to buffefr with size of 100.I want to get something Like Interrupt when the buffer is full.I look for some examples in the internet about the configuration of the IOC bu...

TIM3_IOC_CONF1.png ADC_IOC_CONF1.png ADC_IOC_CONF2.png
TOsso.1 by Associate III
  • 2569 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H753VIT6 SD-card SDR104

Hi,I would like to use this device: STM32H753VIT6 to communicate withan SD-card in SDR104 mode.As I understand it would require an I/O voltage on the card side of 1.8V. This is where I become insecure if the given device can generate this voltage int...

tyassin by Associate III
  • 4158 Views
  • 8 replies
  • 0 kudos

Resolved! STM32H7B0 internal flash gets erased during runtime

Hi,We develop a device based on STM32H7B0. We use this microcontroller with QSPI external flash. In the internal flash we keep our bootloader and in the external flash resides application code. We are now testing our devices and we had 3 cases when t...

ypiotrp by Senior
  • 12842 Views
  • 28 replies
  • 5 kudos

Resolved! STM32C0 and STM32H5 workshop materials

On Thursday, June 29, 2023, I attended the "STM32H5: Ultimate combination of performance, integration and affordability" workshop, which I find very interesting. Workshop participants were informed that the slides and a voucher to order the STM32H5 d...

MirKoz by Associate III
  • 4867 Views
  • 4 replies
  • 3 kudos

STM32U5 SIMD usage (or any other trick to speedup math)

Hello,In my application i need to run double for loop for data inside SRAM. and I would love to speed up my program as much as possible.uint32_t xs = 0, yx = 0, sum =0, i = 0;for(uint32_t x = 0 ; x<600 ; x++){    for(uint32_t y = 0 ; y<600 ; y++)    ...

Linas L by Senior II
  • 2377 Views
  • 2 replies
  • 0 kudos

What if corruption of STM32 option bytes is detected?

Dear experts, A question in relation to OB behavior discussed this thread: https://community.st.com/t5/stm32-mcus-embedded-software/stm32-is-getting-stuck-frozen-and-enables-read-out-protection-at/td-p/615228Is there documentation or App note that ex...

Pavel A. by Super User
  • 2413 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.