STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! input capture on STM32F030

i want use TIM1 CH1 in input capture using DMA.The DMA is set to peripheral to memory and store the data in a buffer of 100 elements.When the transfer of the 100 data is completed i want generate a TIM1 interrupt. Wich kind of interrupt of TIM1 i hav...

STM32F4 RTC ISSUE WHEN COINCELL [VBAT] IS REMOVED

Hi community,I'm having a STM32F407VET6 PCB board where VBAT is connected to a 10 uF decoupling capacitor [Instead of recommended 100 nF capacitor].in order to achieve some backup time when both the coin cell and 3.3V are not connected.My RTC is work...

Dhanoosh by Associate II
  • 6200 Views
  • 9 replies
  • 1 kudos

STM IDE DEBUG PROBLEM

I am using STM32F103C8T6 Blue pill board. When I trying to debug a program.it showing  as shown in picture.

WhatsApp Image 2023-12-09 at 11.33.24 AM.jpeg
sk108615 by Associate
  • 1231 Views
  • 1 replies
  • 0 kudos

Probability of peripheral failure on a STM32H7

 In the context of functional safety application, we are wondering the probability of a status bit failure on a STM32H753.A low-level software is frequently polling on status bits of peripherals. If this peripheral encounter a failure this is obvious...

Gpeti by Senior II
  • 4385 Views
  • 9 replies
  • 5 kudos

HRTIM output is not observed as mentioned in datasheet

Hello Team,I would like to mention an error I’m facing while testing the HRTIM module in STM32G474RE Evaluation Board. Please find the error details below.Evaluation Board Used: STM32G474REIssue details:In the STM32datasheet: stm32g474ce_details.pdf ...

FEngi.1 by Associate II
  • 1018 Views
  • 1 replies
  • 0 kudos

DR register outputs incorrect numbers STM32F407VG

Hey STMcommunity, I am trying to implement a Modbus protocol, however the DR register of the USART i am using does not output the correct numbers.    I am sending the following message to the MCU "11 03 00 04 00 04 07 58" (hex numbers) but get the fo...

Jordi__0-1702039723989.png Jordi__1-1702039866039.png
Jordi_ by Associate
  • 1015 Views
  • 1 replies
  • 0 kudos

Resolved! Strange USB Behaviors

Greetings, Sorry if I am posting in the wrong place.  Maybe someone can point to the correct forum for me.Problem: USB HID 04 Joystick intermittently sends incorrect 12-bit analog data.Micro: STM32F103R8T6Details: A 1/2 Hz signal applied to analog in...

Loren by Associate III
  • 6895 Views
  • 13 replies
  • 1 kudos

STM32H743 Vrefint value is always read as 0xFFFF

Hello to everyone,I have encountered a problem trying to work with ADC data on STM32H743 chip. When I read VREFINT value (19th ADC input channel) I always see 0xFFFF. Data on other channels look slightly more adequate (at least they are changed depen...

OIrin.1 by Associate II
  • 3734 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.