STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FDCAN interrupt lines in the manual...

I got a hard time comprehending about the two interrupt lines in the manual. I can really see a "connection" between certain sources to the interrupt lines, nor can i find a register to connect them. It seems to me, that i only can decide what interr...

say what.jpg
Tobe by Senior III
  • 4874 Views
  • 6 replies
  • 1 kudos

Dual Channel Parallel ADC with DCMIPP

Hi there! I'm looking to interface a dual channel 12bits ADC (TI ADS4222) with an STM32N647L0.Using a 58MHz sampling clock, I will generate two 58MSPS data streams feeding into my STM32. The acquisitions will be short, so the raw data will be around ...

qmace by Associate
  • 600 Views
  • 1 replies
  • 0 kudos

Request for EOL Information – STM32F091CBU6

Dear STMicroelectronics Support Team,I am currently working on a project that uses the STM32F091CBU6 microcontroller. Could you please confirm the current lifecycle status of this part and provide any available information regarding its projected End...

Regarding voltage on I2C SCL, SDA pins dependency on VDD

Hi, I am using STM32U083 for one of our project. We are using the I2C peripheral to communicate with NFC dynamic tag through I2C.In STM32U0 datasheet I found that the I2C pins SCL and SDA are 5V tolerent pins.We need the I2C to work independently of ...

Magvel by Associate II
  • 1177 Views
  • 5 replies
  • 0 kudos

Resolved! FDCAN repeated transmissions - CAN memory altered after TX ?

Heyho,question about FDCAN and repeating / timed transmission of the same messages:(this is neither about TT CAN nor auto re-transmission, but e.g. for messages which need to be sent every 100 ms repeatedly and "manually")After the first setting of t...

LCE by Principal II
  • 898 Views
  • 6 replies
  • 4 kudos

Bank switch does not always work

Hello everyone!I'm facing a problem when trying to switch a bank on STM32H745 MCU. The issue happens only when the debugger is disconnected. Our implementation uses the HAL library to perform Bank switch like this:HAL_FLASH_Unlock(); HAL_FLAS...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.