2025-12-02 3:53 AM - edited 2025-12-02 4:03 AM
Hello,
we have to use the STM32H573 in the 80 Pin WLCSP with temperature Range 3 (to 125°C). So STM32H573MIY3Q was chosen. Due to a mistake we didn't recognized that the internal LDO can't be used. Now we have no space for placing additional components as the inductor to use the SMPS. The STM is on a tiny board which is connected on a baseboard on this is more space for components.
So now we have two options:
In both cases the Questions are:
How has the pins of SMPS to be configured (by hardware) to shut down the SMPS appropriately?
Do we have to use the VCAP as an input?
If STM staff is reading this please get in touch with us immediately. Thanks.
So long
Marwin
Edits: Some minor spellings
2025-12-02 5:50 AM
> Due to a mistake we didn't recognized that the internal LDO can't be used.
?? You're not required to use SMPS.
See "Figure 6. STM32H523/H533/H562/H563/H573 power-supply scheme with LDO" in the following document:
Getting started with STM32H5 MCU hardware development - Application note
> The maximum IDD ist stated with 125,2 mA, does any additional current has to be added?
Is there other stuff on the board that will be taking current? Do you want any margin? If not, just plan for 125 mA.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.