2025-12-02 12:21 AM
Hy,
I received the STM32N6 DK Kit, switched it on - and it crashes immediately. All demos run smoothly, but as soon as I start the AI demo, the display turns grey after approx 2 seconds.
I power the device over USB port with my 65W Laptop Power supply, jumper JP2 set to 3-4 (5V_USB)
When running the DCMIPP_ContinuousMode_FSBL example project, I see a stable, smooth camera image, so apparently no connection issues to the camera.
Any hints?
Best regards
Harald
2025-12-02 2:07 AM
Hello,
there is a similar case which has been discussed, you can refer to: STM32N6570-DK Camera Issue - STMicroelectronics Community
2025-12-02 4:08 AM - edited 2025-12-02 8:49 AM
Thanks a lot for your response. Reflashing the demo hex file "STM32N6570-DK Out-of-the-box demo binary" from https://community.st.com/t5/stm32-mcus-boards-and-hardware/stm32n6570-dk-camera-issue/td-p/830021 seems to solve the issue. My board is running the AI example properly now.
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.