STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 PWM Duty Cycle Setting.

Hello, In my motor control project, I'm reading potentiometer value and set it as a duty cycle value. Initially I'm using "htim1.Instance->CCR1 = 50;" this function for pwm. but this is not giving correct phase voltage. Can anyone please tell me wh...

Resolved! STM32F103RCT6TR

Hi, I am MURALI SELVAM I need a reference schematic for STM32F103RCT6TR. Anybody with a reference schematic for STM32F103RCT6TR, Kindly share me thank you.

murali by Associate III
  • 3605 Views
  • 7 replies
  • 2 kudos

Resolved! STM32F723 DFU Mode - Questions

I have a few questions about the DFU mode on the STM32F723. My goal is to enable users to flash a binary file to the MCU via a USB connection. My implementation is that i placed a 22uF capacitor on the boot0 pin then tied another IO pin (EO) in this ...

Russeree_0-1704836128752.png
Russeree by Associate II
  • 5727 Views
  • 5 replies
  • 2 kudos

Resolved! SPI pin for STM32F429

Hi community, just a single question as confirm.  I am working with stm32f429.From the schematic the hw engineer decided to use the following pin for spi purpose for communicating with an eeprom  Can you confirm that i cannot use those pins for spi p...

SGasp1_0-1704962915971.png
SGasp.1 by Senior
  • 3706 Views
  • 7 replies
  • 0 kudos

Resolved! TCP IP problem using LWIP RAW API in STM32F429ZI

I am developing a terminal device that performs serial communication and Ethernet communication using stm32f429zit6. TCP IP communication is performed between this terminal device and the server, and lwip raw API is being used for TCP IP communicatio...

image1.png image2.png image3.png
joseph05 by Associate III
  • 6935 Views
  • 8 replies
  • 0 kudos

Resolved! Verify in bootloader USART protocol fails

Hello Community,Using the USART commands in boot mode on a STM32H723 CPU, I faced following issues:Extended erase (0x44) and writing memory(0x31) to the flash works fine, if I write ALL bytes in blocks of 256 bytes.But if I do a read memory(0x11) aft...

TomKing by Associate II
  • 8591 Views
  • 14 replies
  • 1 kudos

HRTIM variable PWM glitch on STM32F334R8

Hi,I'm generating a variable duty PWM on HRTIM1, Timer A, unit 1. It is configured to 500 kHz, with a 217 ps resolution.I want to update the duty value every 50 kHz. It works, but on some steps, the duty glitches to high state (it seems that the comp...

MCris4_0-1687441006734.png MCris4_1-1687441041541.png image6952.png
MCris.4 by Associate II
  • 2243 Views
  • 2 replies
  • 0 kudos

Resolved! Confusion about ADC sampling speed and sampled value

Hello.I am very new in using STM32. I am using STM32H747I-DISCO board. For my project, I only need one ADC in differential mode. Previously, I tried to use DMA with ADC but it never worked, even the "ADC dual mode interleaved" example provided by st ...

rakib2023 by Associate III
  • 4365 Views
  • 14 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.