2014-04-16 1:11 AM
Hello
Thehttp://www.st.com/web/catalog/tools/FM116/SC959/SS1532/PF259090
has a few Free I/O Pins. Is there a list of alternate functions of those pins? It's not mentioned in the corresponding documentation DocID025175 Rev 1 I'm trying to evaluate whether the few I/O Pins are suitable for me or not. Regards Chriostoph2014-04-16 1:28 PM
Is there any schematics (resistors, capacitors, Crystal....) showing a reference to connect a separate µC (STM32F429ZI or similar)?
2014-04-16 2:26 PM
[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Minimum%20circuit%20for%20bare%20STM32%20F2%20lqfp64&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=116]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FMinimum%20circuit%20for%20bare%20STM32%20F2%20lqfp64&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=116
Pretty sure thehttp://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00071990.pdf
addresses some of the required connectivity, capacitors, etc2014-04-17 8:29 AM
I tried to connect a separate µC (STM32F429ZIT_LQFP144) as shown in the document attached…
The problem is that when I connect the power source (3V) to the voltage line and I measure it, it gives low voltage (+/-0.2V)….It looks like I have some short circuit.
Can someone tell me if the pins connections are OK?
________________ Attachments : PINS.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I05c&d=%2Fa%2F0X0000000bTM%2FXRhuK6YJoFHiKPyBGm0m_mjUXAskzc2K2PDhIEdUdVU&asPdf=false2014-04-17 8:43 AM
The VCAP pins only need 2.2uF
The NRST pin should definitely not be connected to the supply. What's up with the 10K + 100nF? VSS (107) not VCC PDR_ON (143) connect to VDD Your design offers not method to test signs-of-life, you'd perhaps want to attach a CMOS Serial (not RS232 levels) connection to PA9/PA10 so you can use a terminal or Flash Loader Demonstrator Would probably add a 1uF on the supply2014-04-17 9:33 AM
I've done the changes that you recommended...But I'm still getting small voltage.
It may be caused by some bridges formed during the soldering. Concerning the the external crystals are they mandatory?2014-04-17 9:48 AM
2014-04-17 10:58 AM
I've done the changes that you recommended...But I'm still getting small voltage. It may be caused by some bridges formed during the soldering.Concerning the the external crystals are they mandatory?
I can't speak to your solder skills, make sure you have the part correctly orientated. VCAP pins should be at 1.25V You do not need external crystals, and they will not start if you have them attached. The part starts up from the internal 16 MHz HSI. To get the blinky example working you'd still need a method to inject code, Serial, USB, or JTAG/SWD
2014-04-17 11:16 AM
Concerning the soldering, I used the university Equipment (Microscope to check...); but I'll go back tomorrow to recheck.
When I'll get the voltage problem solved I'll connect to the chip by SWD via the ST link of my STM32F429I-disco2014-04-21 11:47 AM
2014-04-21 12:10 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.