STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32 accelerometer

Posted on April 30, 2014 at 11:54hi, I have a problem. I2C busy flag always set. I am using I2C1 peripherel. this peripherel conected EEPROM, IO expander and Lis302dlI think, problem is attaching EEPROM  or  IO expander. how can I disconnect EEPROM ...

Where can I find all the examples for the STM32F4Discovery?

Posted on April 30, 2014 at 15:25I just purchased an STM32F4Discovery and I'm getting very frustrated before I've even begun working with it. All the website product pages and documentation say that there are many application firmware examples locat...

sandtime by Associate II
  • 4660 Views
  • 5 replies
  • 1 kudos

32F429IDISCOVERY Pinout / Free IO

Posted on April 16, 2014 at 10:11Hello The http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/PF259090has a few Free I/O Pins. Is there a list of alternate functions of those pins? It's not mentioned in the corresponding documentation DocID02517...

sultanof by Associate II
  • 7732 Views
  • 28 replies
  • 0 kudos

STM32F4Discovery with FatFS in SPI mode

Posted on April 27, 2014 at 20:47Hi all, Is someone else tried to implement solution about Fatfs (sd card) on discovery card with SPI communication ? I triedhttp://eliaselectronics.com/reading-sd-cards-with-the-stm32f4-discovery/ with http://elm-cha...

tgoin by Associate II
  • 1460 Views
  • 2 replies
  • 0 kudos

Where do basic System Debug setting happen using STM32Cube

Posted on April 30, 2014 at 20:40I'm working with a project generated by STM32CubeMX. I can see all the generated code that enables the various IPs and all the pin configuration. However, I can't locate where GPIOs are set to be used for SWD/SWO. I ...

kartik by Associate II
  • 2294 Views
  • 4 replies
  • 0 kudos

STM32F401 -- SPI Slave Receiving 32bit word

Posted on April 30, 2014 at 23:57I have a SPI master device that transmits data in 32 bits while NSS is active. Since the STM32F401 SPI can only be configured as a 16bit SPI port, I am wondering if I can still make it work. Will the SPI port continu...

dibs by Associate II
  • 572 Views
  • 0 replies
  • 0 kudos

Facial recogniction and eigenface

Posted on April 30, 2014 at 14:38Guys, Does anyone of you have experience on using eigenface for comparing the image from camera ? Any references ? thanks #cross-post

STM32LXX eeprom initialized data

Posted on April 26, 2014 at 10:33Hi I use STM32L151CC it has embeded EEPROM data 8KB, I now how to write or read from this memory, but I don't now how to initialize data in eeprom when I programming device. Someone knows how to do it? I use GCC comp...

wilkxt by Associate II
  • 915 Views
  • 2 replies
  • 0 kudos

STM32Cube generated project, adding to HAL driver

Posted on April 29, 2014 at 22:22I'm having trouble during the Link stage after adding a component to the HAL driver in my project. I'm using IAR. I generated a project using STM32CubeMX. I then manually added use of the RTC component, by including ...

kartik by Associate II
  • 2363 Views
  • 4 replies
  • 0 kudos

Bootload on STM32f107RCT (64PIN)

Posted on April 29, 2014 at 19:16In AN2606:''Workaround�? For 64-pin packagesNone. The bootloader cannot be used.�? For 100-pin packagesDepending on the used peripheral, the pins for the unused peripherals have to be keptat a high level during the b...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.