STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Resolved! Missing sample points with MC Control Pilot Scope

Hello,I recorded plots using the real time scope of the MC Control Pilot, and I noticed that the generated file does not include all the points. There is a gap between 2 sample points and its recurring in every plot. TIMESTAMPS I_Q_MEAS I_D_MEAS I_Q_...

AnthonyK by Associate III
  • 838 Views
  • 1 replies
  • 0 kudos

Need help with BLDC motor control for ESC

Hi, We are trying to develop a ESC for Drones of smaller size i.e. with low payload... Currently we are using motors of T Motor Make F2004 1700KV model, Ideally we should be achieving motor speeds up to 20000 RPM , We were looking into two of STM ref...

STEVAL-CTM009V1 machine does not rotate and bugs

Hi, [PN]: STEVAL-CTM009V1 with F446RE[VERSION]: 6.3.2[TOOL]: MC SDK[DETAILS]: just can't get the engine to turn[EXPECTED BEHAVIOR]:the engine turns[HOW TO REPRODUCE]: see below...First:There is a bug in RevUp—see the picture below. When changing the ...

Resolved! PC15 as GPIO input on STEVAL-PTOOL4A

Hello,I am trying to use PC15 as GPIO input on the STEVAL-PTOOL4A. I configured it using CubeMX with pull-down resistor however the pin status is not changing in the software. I am sure my switch works well (checked on oscilloscope) and the LSE is di...

AnthonyK_0-1743667452123.png
AnthonyK by Associate III
  • 1125 Views
  • 2 replies
  • 0 kudos

Resolved! MC-SDK position control setting

I started working successfully with MC_SDK 6.3.2. I am doing position control application with BLDC motor. In "ST Motor Pilot v1.2.12-PositionControlApp" I want to set "Terget Position" value to values ​​bigger than the set max value. From which file...

atemur by Associate
  • 1412 Views
  • 2 replies
  • 1 kudos

Resolved! Torque command sequence

I want to confirm if the below 3 commands 1,2,3 can be given sequentially or any delay required between them. These 3 commands i am giving when a key is pressed. if(IDLE == MC_GetSTMStateMotor1()) { g_qdreference_s.q = 1000; MC_SetCurrentRefere...

STUser34 by Associate III
  • 972 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.